sl_bt_evt_gatt_characteristicGATT Client#

Indicates that a GATT characteristic in the remote GATT database was discovered.

Data Structures

struct  

sl_bt_evt_gatt_characteristic_s

Data structure of the characteristic event.

Macros

#define  

sl_bt_evt_gatt_characteristic_id   0x020900a0

Identifier of the characteristic event.

Detailed Description#

Indicates that a GATT characteristic in the remote GATT database was discovered.

This event is generated after issuing either the sl_bt_gatt_discover_characteristics or sl_bt_gatt_discover_characteristics_by_uuid command.


Data Structure Documentation#

◆sl_bt_evt_gatt_characteristic_s#

struct sl_bt_evt_gatt_characteristic_s

Data structure of the characteristic event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

characteristic

GATT characteristic handle

uint8_t

properties

Characteristic properties

uint8array

uuid

Characteristic UUID in little endian format