sl_bt_evt_gatt_descriptorGATT Client#

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

Data Structures

struct  

sl_bt_evt_gatt_descriptor_s

Data structure of the descriptor event.

Macros

#define  

sl_bt_evt_gatt_descriptor_id   0x030900a0

Identifier of the descriptor event.

Detailed Description#

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

It is generated after issuing the sl_bt_gatt_discover_descriptors command.


Data Structure Documentation#

◆sl_bt_evt_gatt_descriptor_s#

struct sl_bt_evt_gatt_descriptor_s

Data structure of the descriptor event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

descriptor

GATT characteristic descriptor handle

uint8array

uuid

Descriptor UUID in little endian format