sl_bt_evt_gatt_descriptor_valueGATT Client#

Indicates that the value of a descriptor in the remote GATT server was received.

Data Structures

struct  

sl_bt_evt_gatt_descriptor_value_s

Data structure of the descriptor_value event.

Macros

#define  

sl_bt_evt_gatt_descriptor_value_id   0x050900a0

Identifier of the descriptor_value event.

Detailed Description#

Indicates that the value of a descriptor in the remote GATT server was received.

This event is generated by the sl_bt_gatt_read_descriptor_value command.


Data Structure Documentation#

◆sl_bt_evt_gatt_descriptor_value_s#

struct sl_bt_evt_gatt_descriptor_value_s

Data structure of the descriptor_value event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

descriptor

GATT characteristic descriptor handle

uint16_t

offset

Value offset

uint8array

value

Descriptor value