sl_bt_evt_gatt_mtu_exchangedGATT Client#

Indicates that an ATT_MTU exchange procedure is completed.

Data Structures

struct  

sl_bt_evt_gatt_mtu_exchanged_s

Data structure of the mtu_exchanged event.

Macros

#define  

sl_bt_evt_gatt_mtu_exchanged_id   0x000900a0

Identifier of the mtu_exchanged event.

Detailed Description#

Indicates that an ATT_MTU exchange procedure is completed.

The mtu parameter describes new MTU size. MTU size 23 is used before this event is received.


Data Structure Documentation#

◆sl_bt_evt_gatt_mtu_exchanged_s#

struct sl_bt_evt_gatt_mtu_exchanged_s

Data structure of the mtu_exchanged event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint16_t

mtu

Exchanged ATT_MTU