Modules#
sl_bt_evt_sync_closed#
Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.
The synchronization establishment procedure can be canceled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.
Typedefs#
typedef struct sl_bt_evt_sync_closed_s
Macros#
#define
sl_bt_evt_sync_closed_id 0x014200a0
Identifier of the closed event.
Typedef Documentation#
sl_bt_evt_sync_closed_t#
typedef struct sl_bt_evt_sync_closed_s sl_bt_evt_sync_closed_t
Definition at line
4770
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h