Data structure of the data event.

Public Attributes#

uint16_t
int8_t
int8_t

Public Attribute Documentation#

sync#

uint16_t sl_bt_evt_sync_data_s::sync

Periodic advertising synchronization handle


Definition at line 4725 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

tx_power#

int8_t sl_bt_evt_sync_data_s::tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable


Definition at line 4726 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_sync_data_s::rssi

Signal strength indicator (RSSI) in the latest received packet. Units: dBm

  • Range: -127 to +20


Definition at line 4730 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

data_status#

uint8_t sl_bt_evt_sync_data_s::data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come


Definition at line 4733 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_sync_data_s::data

Periodic advertising data


Definition at line 4739 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h