Data structure of the opened event.

Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

address#

bd_addr sl_bt_evt_connection_opened_s::address

Remote device address


address_type#

uint8_t sl_bt_evt_connection_opened_s::address_type

Enum sl_bt_gap_address_type_t. Remote device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


master#

uint8_t sl_bt_evt_connection_opened_s::master

Device role in connection. Values:

  • 0: Peripheral

  • 1: Central


connection#

uint8_t sl_bt_evt_connection_opened_s::connection

Handle for new connection


bonding#

uint8_t sl_bt_evt_connection_opened_s::bonding

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle


advertiser#

uint8_t sl_bt_evt_connection_opened_s::advertiser

The local advertising set that this connection was opened to. Values:

  • SL_BT_INVALID_ADVERTISING_SET_HANDLE (0xff): Invalid value or not applicable. Ignore this field

  • Other: The advertising set handle


sync#

uint16_t sl_bt_evt_connection_opened_s::sync

The sync handle if the local device is in the peripheral-role and the connection was opened via a Periodic Advertising with Responses (PAwR) train that the local device has synchronized to. Values:

  • SL_BT_INVALID_SYNC_HANDLE (0xffff): The connection was not opened over a PAwR train that the local device is synchronized to

  • Other: The sync handle for the PAwR train that was used to open the connection