Sync PAST#
Sync PAST.
Transfer the synchronization information of a synchronized periodic advertising train to a remote device using Periodic Advertising Synchronization Transfer (PAST) over a connection.
Functions#
sl_status_t
sl_bt_sync_past_transfer(uint8_t connection, uint16_t service_data, uint16_t sync)
Macros#
#define
sl_bt_cmd_sync_past_transfer_id 0x005b0020
#define
sl_bt_rsp_sync_past_transfer_id 0x005b0020
Function Documentation#
sl_bt_sync_past_transfer#
sl_status_t sl_bt_sync_past_transfer (uint8_t connection, uint16_t service_data, uint16_t sync)
Parameters
[in] | connection | Connection handle of the connection used to transmit the sync transfer |
[in] | service_data | A value provided by the application for use by the peer device. |
[in] | sync | Handle of the periodic advertising synchronization to transfer |
Transfer the synchronization information of a periodic advertising train for which a sync has been established.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
5456
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_cmd_sync_past_transfer_id#
#define sl_bt_cmd_sync_past_transfer_idValue:
0x005b0020
Definition at line
5438
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_sync_past_transfer_id#
#define sl_bt_rsp_sync_past_transfer_idValue:
0x005b0020
Definition at line
5439
of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h