GATT Database#
GATT Database.
These commands and events are used for managing the local GATT database.
Many commands in this class return the handles of created attributes. These handles may change during commit if attributes are not created in the order they present in the database. For example, when creating a new service using the sl_bt_gattdb_add_service command, the service declaration handle returned from this command becomes invalid later when an attribute is added or removed in front of this service. If the user requires that the attribute handles returned from these commands must remain valid after the database update has been committed, attributes must be created in the order they present in the database.
Modules#
GATT Attribute Security Requirement Flags
GATT Characteristic Property Flags
GATT Descriptor Property Flags
Enumerations#
This enum defines GATT service types.
This enum defines characteristic and descriptor value types.
Functions#
Macros#
Enumeration Documentation#
sl_bt_gattdb_service_type_t#
sl_bt_gattdb_service_type_t
This enum defines GATT service types.
Enumerator | |
---|---|
sl_bt_gattdb_primary_service | (0x0) Primary service |
sl_bt_gattdb_secondary_service | (0x1) Secondary service |
7915
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_value_type_t#
sl_bt_gattdb_value_type_t
This enum defines characteristic and descriptor value types.
Enumerator | |
---|---|
sl_bt_gattdb_fixed_length_value | (0x1) A fixed-length value managed by the local GATT server for responding the read and write requests of remote GATT clients |
sl_bt_gattdb_variable_length_value | (0x2) A variable-length value managed by the local GATT server for responding the read and write requests of remote GATT clients |
sl_bt_gattdb_user_managed_value | (0x3) A value managed by the user application for responding the read and write requests of remote GATT clients. |
7924
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Function Documentation#
sl_bt_gattdb_new_session#
sl_status_t sl_bt_gattdb_new_session (uint16_t * session)
[out] | session | The database update session ID |
Start a new GATT database update session. If the operation is successful, the Bluetooth stack returns a session ID, with which the GATT database can be updated by calling other database management APIs of this class. Changes in the database are not immediately saved. Unsaved changes are invisible to a connected remote GATT client.
After all changes were performed successfully, commit the changes using the sl_bt_gattdb_commit command. The Bluetooth stack will save the changes and handle GATT caching as needed. Unsaved database changes can also be canceled by calling the sl_bt_gattdb_abort command. In either case, after a commit or abort command is called, the current session is closed and the session ID becomes invalid.
Only one session is allowed at a time. Error SL_STATUS_ALREADY_EXISTS is returned if another session has been started already.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8082
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_service#
sl_status_t sl_bt_gattdb_add_service (uint16_t session, uint8_t type, uint8_t property, size_t uuid_len, const uint8_t * uuid, uint16_t * service)
[in] | session | The database update session ID |
[in] | type | Enum sl_bt_gattdb_service_type_t. The service type. Values:
|
[in] | property | Service properties. Value: 0 or bit flag SL_BT_GATTDB_ADVERTISED_SERVICE |
[in] | uuid_len | Length of data in |
[in] | uuid | The service UUID in little endian format |
[out] | service | The service declaration attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add a service into the local GATT database. When successful, the service is appended to the service list and is in stopped state. Use sl_bt_gattdb_start_service command to set it visible to remote GATT clients.
You are not allowed to add the Generic Attribute Profile service. If the application needs GATT caching, enable the feature in the configuration of this component and the GATT server will handle GATT caching according to the procedures specified by the Bluetooth core specification.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8111
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_remove_service#
sl_status_t sl_bt_gattdb_remove_service (uint16_t session, uint16_t service)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service |
Remove a service and its characteristics from the local GATT database.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8128
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_included_service#
sl_status_t sl_bt_gattdb_add_included_service (uint16_t session, uint16_t service, uint16_t included_service, uint16_t * attribute)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service which the included-service attribute is added to |
[in] | included_service | The service declaration attribute handle of the service to be included |
[out] | attribute | The included-service attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add an included-service attribute to a service.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8146
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_remove_included_service#
sl_status_t sl_bt_gattdb_remove_included_service (uint16_t session, uint16_t attribute)
[in] | session | The database update session ID |
[in] | attribute | The included-service attribute handle |
Remove an included-service attribute from a service.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8161
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_uuid16_characteristic#
sl_status_t sl_bt_gattdb_add_uuid16_characteristic (uint16_t session, uint16_t service, uint16_t property, uint16_t security, uint8_t flag, sl_bt_uuid_16_t uuid, uint8_t value_type, uint16_t maxlen, size_t value_len, const uint8_t * value, uint16_t * characteristic)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service which the characteristic is added to |
[in] | property | Characteristic value properties. Value: bitmask of GATT Characteristic Property Flags |
[in] | security | Security requirement. Value: 0 or bitmask of GATT Attribute Security Requirement Flags. A security requirement flag for a property is ignored if the property is not set for the characteristic value. |
[in] | flag | Option flags. Value: 0 or bitmask of GATT Database Flags. |
[in] | uuid | The 16-bits UUID in little endian format |
[in] | value_type | Enum sl_bt_gattdb_value_type_t. The value type. Values:
|
[in] | maxlen | The maximum length of the characteristic value. Ignored if |
[in] | value_len | Length of data in |
[in] | value | The initial characteristic value. Length of this value must be less than or equal to |
[out] | characteristic | The characteristic value attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add a 16-bits UUID characteristic to a service. On success, the characteristic is appended to the characteristic list of the service and it inherits the started or stopped state of the service. In addition, it can be started and stopped separately with the sl_bt_gattdb_start_characteristic and sl_bt_gattdb_stop_characteristic commands.
If the flag
parameter does not set SL_BT_GATTDB_NO_AUTO_CCCD, the stack will automatically add a Client Characteristic Configuration descriptor to this characteristic when it has the notify or indicate property. If SL_BT_GATTDB_NO_AUTO_CCCD is set, the user application should add the descriptor separately as needed.
A Characteristic Extended Properties descriptor is automatically added if the reliable write property is set.
Use the sl_bt_gattdb_add_uuid128_characteristic command to add a 128-bits UUID characteristic.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8220
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_uuid128_characteristic#
sl_status_t sl_bt_gattdb_add_uuid128_characteristic (uint16_t session, uint16_t service, uint16_t property, uint16_t security, uint8_t flag, uuid_128 uuid, uint8_t value_type, uint16_t maxlen, size_t value_len, const uint8_t * value, uint16_t * characteristic)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service which the characteristic is added to |
[in] | property | Characteristic value properties. Value: bitmask of GATT Characteristic Property Flags |
[in] | security | Security requirement. Value: 0 or bitmask of GATT Attribute Security Requirement Flags. A security requirement flag for a property is ignored if the property is not set for the characteristic value. |
[in] | flag | Option flags. Value: 0 or bitmask of GATT Database Flags. |
[in] | uuid | The 128-bits UUID in little endian format |
[in] | value_type | Enum sl_bt_gattdb_value_type_t. The value type. Values:
|
[in] | maxlen | The maximum length of the characteristic value. Ignored if |
[in] | value_len | Length of data in |
[in] | value | The initial characteristic value. Length of this value must be less than or equal to |
[out] | characteristic | The characteristic value attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add a 128-bits UUID characteristic to a service. When successful, the characteristic is appended to the characteristic list of the service and inherits the started or stopped state of the service. Additionally, it can be started and stopped separately with the sl_bt_gattdb_start_characteristic and sl_bt_gattdb_stop_characteristic commands.
If the flag
parameter does not set SL_BT_GATTDB_NO_AUTO_CCCD, the stack will automatically add a Client Characteristic Configuration descriptor to this characteristic when it has the notify or indicate property. If SL_BT_GATTDB_NO_AUTO_CCCD is set, the user application should add the descriptor separately as needed.
A Characteristic Extended Properties descriptor is automatically added if the reliable write property is set.
Use the sl_bt_gattdb_add_uuid16_characteristic command to add a 16-bits UUID characteristic.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8288
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_remove_characteristic#
sl_status_t sl_bt_gattdb_remove_characteristic (uint16_t session, uint16_t characteristic)
[in] | session | The database update session ID |
[in] | characteristic | The characteristic value attribute handle of the characteristic |
Remove a characteristic and its descriptors from a service.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8311
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_uuid16_descriptor#
sl_status_t sl_bt_gattdb_add_uuid16_descriptor (uint16_t session, uint16_t characteristic, uint16_t property, uint16_t security, sl_bt_uuid_16_t uuid, uint8_t value_type, uint16_t maxlen, size_t value_len, const uint8_t * value, uint16_t * descriptor)
[in] | session | The database update session ID |
[in] | characteristic | The characteristic value attribute handle of the characteristic the descriptor is added to |
[in] | property | The descriptor properties. Value: bitmask of GATT Descriptor Property Flags |
[in] | security | Security requirement. Value: 0 or bitmask of GATT Attribute Security Requirement Flags. A security requirement flag for a property is ignored if the property is not set for the descriptor. |
[in] | uuid | The 16-bits UUID in little endian format |
[in] | value_type | Enum sl_bt_gattdb_value_type_t. The value type. Ignored if this is a Client Characteristic Configuration descriptor. Values:
|
[in] | maxlen | The maximum length of the descriptor value. Ignored if |
[in] | value_len | Length of data in |
[in] | value | The initial descriptor value. Length of this value must be less than or equal to |
[out] | descriptor | The descriptor attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add a 16-bits UUID descriptor to a characteristic. When successful, the descriptor is appended to the descriptor list of the characteristic and inherits the started or stopped state of the characteristic.
This command does not support adding Characteristic Extended Properties descriptors. This descriptor is automatically added if the characteristic value has the reliable-write property or when a Characteristic User Description descriptor is added and the user description has the write property.
Use the sl_bt_gattdb_add_uuid128_descriptor command to add a 128-bits UUID descriptor.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8365
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_add_uuid128_descriptor#
sl_status_t sl_bt_gattdb_add_uuid128_descriptor (uint16_t session, uint16_t characteristic, uint16_t property, uint16_t security, uuid_128 uuid, uint8_t value_type, uint16_t maxlen, size_t value_len, const uint8_t * value, uint16_t * descriptor)
[in] | session | The database update session ID |
[in] | characteristic | The characteristic value attribute handle of the characteristic the descriptor is added to |
[in] | property | Bitmask of characteristic descriptor properties |
[in] | security | Security requirement. Value: 0 or bitmask of GATT Attribute Security Requirement Flags. A security requirement flag for a property is ignored if the property is not set for the descriptor. |
[in] | uuid | The 128-bits UUID in little endian format |
[in] | value_type | Enum sl_bt_gattdb_value_type_t. The value type. Ignored if this is a Client Characteristic Configuration descriptor. Values:
|
[in] | maxlen | The maximum length of the descriptor value. Ignored if |
[in] | value_len | Length of data in |
[in] | value | The initial descriptor value. Length of this value must be less than or equal to |
[out] | descriptor | The descriptor attribute handle. This handle is ensured valid in current session. It may change after the session if attributes have been inserted or deleted in front of it. |
Add a 128-bits UUID descriptor to a characteristic. When successful, the descriptor is appended to the descriptor list of the characteristic and inherits the started or stopped state of the characteristic.
This command does not support adding Characteristic Extended Properties descriptors. This descriptor is automatically added if the characteristic value has the reliable-write property or when a Characteristic User Description descriptor is added and the user description has the write property.
Use the sl_bt_gattdb_add_uuid16_descriptor command to add a 16-bits UUID descriptor.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8426
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_remove_descriptor#
sl_status_t sl_bt_gattdb_remove_descriptor (uint16_t session, uint16_t descriptor)
[in] | session | The database update session ID |
[in] | descriptor | The descriptor handle |
Remove a descriptor from a characteristic.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8447
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_start_service#
sl_status_t sl_bt_gattdb_start_service (uint16_t session, uint16_t service)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service |
Start a service, so that the service and its attributes including characteristics and descriptors become visible to remote GATT clients after this change has been committed.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8462
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_stop_service#
sl_status_t sl_bt_gattdb_stop_service (uint16_t session, uint16_t service)
[in] | session | The database update session ID |
[in] | service | The service declaration attribute handle of the service |
Stop a service, so that the service and its attributes including characteristics and descriptors become invisible to remote GATT clients after this change has been committed.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8476
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_start_characteristic#
sl_status_t sl_bt_gattdb_start_characteristic (uint16_t session, uint16_t characteristic)
[in] | session | The database update session ID |
[in] | characteristic | The characteristic value attribute handle of the characteristic |
Start a characteristic, so that the characteristic and its attributes become visible to remote GATT clients after this change has been committed. SL_STATUS_INVALID_STATE error is returned if the parent service is not started.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8492
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_stop_characteristic#
sl_status_t sl_bt_gattdb_stop_characteristic (uint16_t session, uint16_t characteristic)
[in] | session | The database update session ID |
[in] | characteristic | The characteristic value attribute handle of the characteristic |
Stop a characteristic, so that the characteristic and its attributes become invisible to remote GATT clients after this change has been committed.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8507
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_commit#
sl_status_t sl_bt_gattdb_commit (uint16_t session)
[in] | session | The database update session ID |
Save all changes performed in the current session and close the session. The stack will assign final handles to new and affected attributes and handle GATT caching as needed. The stack removes the client characteristic configurations of non-connected GATT clients except the service-changed configuration. For connected GATT clients during this database change, the stack removes the configurations to the removed characteristics. The session ID, temporary attribute handles returned during this session, and other existing attribute handles that are after newly added or removed attributes are invalidated.
Some attribute handles returned in this session may become invalid if attributes are not created in the order they present in the database. In this case, attribute handle cache of the database in the user application must be refreshed to avoid accidentally using an invalidated handle in subsequent operations.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8533
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_gattdb_abort#
sl_status_t sl_bt_gattdb_abort (uint16_t session)
[in] | session | The database update session ID |
Cancel all changes performed in the current session and close the session. The database remains in the same state it was in just before the session was started. The session ID and all temporary attribute handles returned during this session are invalidated.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8547
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_cmd_gattdb_new_session_id#
#define sl_bt_cmd_gattdb_new_session_idValue:
0x00460020
7877
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_service_id#
#define sl_bt_cmd_gattdb_add_service_idValue:
0x01460020
7878
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_remove_service_id#
#define sl_bt_cmd_gattdb_remove_service_idValue:
0x02460020
7879
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_included_service_id#
#define sl_bt_cmd_gattdb_add_included_service_idValue:
0x03460020
7880
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_remove_included_service_id#
#define sl_bt_cmd_gattdb_remove_included_service_idValue:
0x04460020
7881
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_uuid16_characteristic_id#
#define sl_bt_cmd_gattdb_add_uuid16_characteristic_idValue:
0x05460020
7882
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_uuid128_characteristic_id#
#define sl_bt_cmd_gattdb_add_uuid128_characteristic_idValue:
0x06460020
7883
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_remove_characteristic_id#
#define sl_bt_cmd_gattdb_remove_characteristic_idValue:
0x07460020
7884
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_uuid16_descriptor_id#
#define sl_bt_cmd_gattdb_add_uuid16_descriptor_idValue:
0x08460020
7885
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_add_uuid128_descriptor_id#
#define sl_bt_cmd_gattdb_add_uuid128_descriptor_idValue:
0x09460020
7886
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_remove_descriptor_id#
#define sl_bt_cmd_gattdb_remove_descriptor_idValue:
0x0a460020
7887
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_start_service_id#
#define sl_bt_cmd_gattdb_start_service_idValue:
0x0b460020
7888
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_stop_service_id#
#define sl_bt_cmd_gattdb_stop_service_idValue:
0x0c460020
7889
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_start_characteristic_id#
#define sl_bt_cmd_gattdb_start_characteristic_idValue:
0x0d460020
7890
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_stop_characteristic_id#
#define sl_bt_cmd_gattdb_stop_characteristic_idValue:
0x0e460020
7891
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_commit_id#
#define sl_bt_cmd_gattdb_commit_idValue:
0x0f460020
7892
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_gattdb_abort_id#
#define sl_bt_cmd_gattdb_abort_idValue:
0x10460020
7893
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_new_session_id#
#define sl_bt_rsp_gattdb_new_session_idValue:
0x00460020
7894
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_service_id#
#define sl_bt_rsp_gattdb_add_service_idValue:
0x01460020
7895
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_remove_service_id#
#define sl_bt_rsp_gattdb_remove_service_idValue:
0x02460020
7896
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_included_service_id#
#define sl_bt_rsp_gattdb_add_included_service_idValue:
0x03460020
7897
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_remove_included_service_id#
#define sl_bt_rsp_gattdb_remove_included_service_idValue:
0x04460020
7898
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_uuid16_characteristic_id#
#define sl_bt_rsp_gattdb_add_uuid16_characteristic_idValue:
0x05460020
7899
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_uuid128_characteristic_id#
#define sl_bt_rsp_gattdb_add_uuid128_characteristic_idValue:
0x06460020
7900
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_remove_characteristic_id#
#define sl_bt_rsp_gattdb_remove_characteristic_idValue:
0x07460020
7901
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_uuid16_descriptor_id#
#define sl_bt_rsp_gattdb_add_uuid16_descriptor_idValue:
0x08460020
7902
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_add_uuid128_descriptor_id#
#define sl_bt_rsp_gattdb_add_uuid128_descriptor_idValue:
0x09460020
7903
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_remove_descriptor_id#
#define sl_bt_rsp_gattdb_remove_descriptor_idValue:
0x0a460020
7904
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_start_service_id#
#define sl_bt_rsp_gattdb_start_service_idValue:
0x0b460020
7905
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_stop_service_id#
#define sl_bt_rsp_gattdb_stop_service_idValue:
0x0c460020
7906
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_start_characteristic_id#
#define sl_bt_rsp_gattdb_start_characteristic_idValue:
0x0d460020
7907
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_stop_characteristic_id#
#define sl_bt_rsp_gattdb_stop_characteristic_idValue:
0x0e460020
7908
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_commit_id#
#define sl_bt_rsp_gattdb_commit_idValue:
0x0f460020
7909
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_gattdb_abort_id#
#define sl_bt_rsp_gattdb_abort_idValue:
0x10460020
7910
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h