OTS Object Server Client database item.

Public Attributes#

uint16_t

The connection handle that identifies the client.

Selected Current Object ID.

Pointer to Current Object Properties (or NULL if not specified)

sl_bt_ots_object_size_t *

Pointer to Current Object Size (or NULL if not specified)

Subscription status for indication to OACP, OLCP and Object Change characteristics.

Current object transfer channel (L2CAP channel)

uint16_t

SDU of the current L2CAP transfer.

uint16_t

PDU of the current L2CAP transfer.

sl_bt_ots_oacp_opcode_t

Current transfer related operation (Read or Write)

Object used in the current transfer.

Public Attribute Documentation#

connection_handle#

uint16_t sl_bt_ots_server_client_db_entry_t::connection_handle

The connection handle that identifies the client.


Definition at line 261 of file common/ots/inc/sl_bt_ots_server.h

current_object#

sl_bt_ots_object_id_t sl_bt_ots_server_client_db_entry_t::current_object

Selected Current Object ID.


Definition at line 262 of file common/ots/inc/sl_bt_ots_server.h

current_object_properties#

sl_bt_ots_object_properties_t* sl_bt_ots_server_client_db_entry_t::current_object_properties

Pointer to Current Object Properties (or NULL if not specified)


Definition at line 263 of file common/ots/inc/sl_bt_ots_server.h

current_object_size#

sl_bt_ots_object_size_t* sl_bt_ots_server_client_db_entry_t::current_object_size

Pointer to Current Object Size (or NULL if not specified)


Definition at line 264 of file common/ots/inc/sl_bt_ots_server.h

subscription_status#

sl_bt_ots_subscription_status_t sl_bt_ots_server_client_db_entry_t::subscription_status

Subscription status for indication to OACP, OLCP and Object Change characteristics.


Definition at line 265 of file common/ots/inc/sl_bt_ots_server.h

l2cap_transfer#

sl_bt_l2cap_transfer_transfer_t sl_bt_ots_server_client_db_entry_t::l2cap_transfer

Current object transfer channel (L2CAP channel)


Definition at line 266 of file common/ots/inc/sl_bt_ots_server.h

l2cap_transfer_sdu#

uint16_t sl_bt_ots_server_client_db_entry_t::l2cap_transfer_sdu

SDU of the current L2CAP transfer.


Definition at line 267 of file common/ots/inc/sl_bt_ots_server.h

l2cap_transfer_pdu#

uint16_t sl_bt_ots_server_client_db_entry_t::l2cap_transfer_pdu

PDU of the current L2CAP transfer.


Definition at line 268 of file common/ots/inc/sl_bt_ots_server.h

operation_in_progress#

sl_bt_ots_oacp_opcode_t sl_bt_ots_server_client_db_entry_t::operation_in_progress

Current transfer related operation (Read or Write)


Definition at line 269 of file common/ots/inc/sl_bt_ots_server.h

object_in_use#

sl_bt_ots_object_id_t sl_bt_ots_server_client_db_entry_t::object_in_use

Object used in the current transfer.


Definition at line 270 of file common/ots/inc/sl_bt_ots_server.h