Data structure of the characteristic_value event.

Public Attributes#

uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_characteristic_value_s::connection

Connection handle


Definition at line 7201 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

characteristic#

uint16_t sl_bt_evt_gatt_characteristic_value_s::characteristic

GATT characteristic handle. This value is normally received from the gatt_characteristic event.


Definition at line 7202 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

att_opcode#

uint8_t sl_bt_evt_gatt_characteristic_value_s::att_opcode

Enum sl_bt_gatt_att_opcode_t. Attribute opcode, which indicates the GATT transaction used.


Definition at line 7205 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

offset#

uint16_t sl_bt_evt_gatt_characteristic_value_s::offset

Value offset


Definition at line 7208 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

value#

uint8array sl_bt_evt_gatt_characteristic_value_s::value

Characteristic value


Definition at line 7209 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h