Data structure of the service event.

Public Attributes#

uint8_t
uint32_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_service_s::connection

Connection handle


Definition at line 7109 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

service#

uint32_t sl_bt_evt_gatt_service_s::service

GATT service handle


Definition at line 7110 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

uuid#

uint8array sl_bt_evt_gatt_service_s::uuid

Service UUID in little endian format


Definition at line 7111 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h