sl_bt_evt_pawr_sync_subevent_report#
Reports that the device's radio has received a periodic advertisement in a subevent of an active PAwR train.
This event reports also empty advertisements, i.e., advertisements that contained no payload data. In this case the data
parameter has zero length.
Modules#
sl_bt_evt_pawr_sync_subevent_report_s
Typedefs#
Macros#
#define
sl_bt_evt_pawr_sync_subevent_report_id 0x025400a0
Identifier of the subevent_report event.
Typedef Documentation#
sl_bt_evt_pawr_sync_subevent_report_t#
typedef struct sl_bt_evt_pawr_sync_subevent_report_s sl_bt_evt_pawr_sync_subevent_report_t
Definition at line
4951
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_pawr_sync_subevent_report_id#
#define sl_bt_evt_pawr_sync_subevent_report_idValue:
0x025400a0
Identifier of the subevent_report event.
Definition at line
4894
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h