CTE Receiver#

CTE Receiver.

Commands and events in this class manage Constant Tone Extension (CTE) receiving.

CTE feature is only supported by specific devices. Commands from this class will return SL_STATUS_NOT_SUPPORTED on devices that do not support CTE.

Modules#

CTE type flags for limiting periodic advertising synchronization

sl_bt_evt_cte_receiver_dtm_iq_report

sl_bt_evt_cte_receiver_connection_iq_report

sl_bt_evt_cte_receiver_connectionless_iq_report

sl_bt_evt_cte_receiver_silabs_iq_report

Functions#

sl_status_t
sl_bt_cte_receiver_set_dtm_parameters(uint8_t cte_length, uint8_t cte_type, uint8_t slot_durations, size_t switching_pattern_len, const uint8_t *switching_pattern)
sl_status_t
sl_status_t
sl_bt_cte_receiver_set_default_sync_receive_parameters(uint8_t mode, uint16_t skip, uint16_t timeout, uint8_t sync_cte_type, uint8_t reporting_mode)
sl_status_t
sl_bt_cte_receiver_set_sync_receive_parameters(uint8_t connection, uint8_t mode, uint16_t skip, uint16_t timeout, uint8_t sync_cte_type, uint8_t reporting_mode)
sl_status_t
sl_status_t
sl_bt_cte_receiver_enable_connection_cte(uint8_t connection, uint16_t interval, uint8_t cte_length, uint8_t cte_type, uint8_t slot_durations, size_t switching_pattern_len, const uint8_t *switching_pattern)
sl_status_t
sl_status_t
sl_bt_cte_receiver_enable_connectionless_cte(uint16_t sync, uint8_t slot_durations, uint8_t cte_count, size_t switching_pattern_len, const uint8_t *switching_pattern)
sl_status_t
sl_bt_cte_receiver_enable_silabs_cte(uint8_t slot_durations, uint8_t cte_count, size_t switching_pattern_len, const uint8_t *switching_pattern)

Macros#

#define
sl_bt_cmd_cte_receiver_set_dtm_parameters_id 0x05450020
#define
sl_bt_cmd_cte_receiver_clear_dtm_parameters_id 0x06450020
#define
sl_bt_cmd_cte_receiver_set_sync_cte_type_id 0x09450020
#define
sl_bt_cmd_cte_receiver_set_default_sync_receive_parameters_id 0x0a450020
#define
sl_bt_cmd_cte_receiver_set_sync_receive_parameters_id 0x0b450020
#define
sl_bt_cmd_cte_receiver_configure_id 0x00450020
#define
sl_bt_cmd_cte_receiver_enable_connection_cte_id 0x01450020
#define
sl_bt_cmd_cte_receiver_disable_connection_cte_id 0x02450020
#define
sl_bt_cmd_cte_receiver_enable_connectionless_cte_id 0x03450020
#define
sl_bt_cmd_cte_receiver_disable_connectionless_cte_id 0x04450020
#define
sl_bt_cmd_cte_receiver_enable_silabs_cte_id 0x07450020
#define
sl_bt_cmd_cte_receiver_disable_silabs_cte_id 0x08450020
#define
sl_bt_rsp_cte_receiver_set_dtm_parameters_id 0x05450020
#define
sl_bt_rsp_cte_receiver_clear_dtm_parameters_id 0x06450020
#define
sl_bt_rsp_cte_receiver_set_sync_cte_type_id 0x09450020
#define
sl_bt_rsp_cte_receiver_set_default_sync_receive_parameters_id 0x0a450020
#define
sl_bt_rsp_cte_receiver_set_sync_receive_parameters_id 0x0b450020
#define
sl_bt_rsp_cte_receiver_configure_id 0x00450020
#define
sl_bt_rsp_cte_receiver_enable_connection_cte_id 0x01450020
#define
sl_bt_rsp_cte_receiver_disable_connection_cte_id 0x02450020
#define
sl_bt_rsp_cte_receiver_enable_connectionless_cte_id 0x03450020
#define
sl_bt_rsp_cte_receiver_disable_connectionless_cte_id 0x04450020
#define
sl_bt_rsp_cte_receiver_enable_silabs_cte_id 0x07450020
#define
sl_bt_rsp_cte_receiver_disable_silabs_cte_id 0x08450020

Function Documentation#

sl_bt_cte_receiver_set_dtm_parameters#

sl_status_t sl_bt_cte_receiver_set_dtm_parameters (uint8_t cte_length, uint8_t cte_type, uint8_t slot_durations, size_t switching_pattern_len, const uint8_t * switching_pattern)
Parameters
[in]cte_length

Expected CTE length in 8 us units

  • 0: No CTE

  • 0x02 to 0x14: Expected CTE length

Default: 0 (no CTE)

[in]cte_type

Expected CTE type

  • 0: Expect AoA CTE

  • 1: Expect AoD CTE with 1 us slots

  • 2: Expect AoD CTE with 2 us slots

Default: 0

[in]slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each

Default: 1

[in]switching_pattern_len

Length of data in switching_pattern

[in]switching_pattern

Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over. This can be an empty array if CTE is unused.

Set CTE-related parameters of LE receiver test.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 14115 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_clear_dtm_parameters#

sl_status_t sl_bt_cte_receiver_clear_dtm_parameters ()

Clear CTE-related parameters that were previously set for LE receiver test. Default values will be restored for these parameters.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14130 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_set_sync_cte_type#

sl_status_t sl_bt_cte_receiver_set_sync_cte_type (uint8_t sync_cte_type)
Parameters
[in]sync_cte_type

Sync CTE type flags. This value can be a bitmask of multiple flags from CTE type flags for limiting periodic advertising synchronization. Flags:

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOA (0x01, bit 0): Do not sync to packets with an AoA Constant Tone Extension

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_1_US (0x02, bit 1): Do not sync to packets with an AoD Constant Tone Extension with 1 us slots

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_2_US (0x04, bit 2): Do not sync to packets with an AoD Constant Tone Extension with 2 us slots

  • SL_BT_CTE_RECEIVER_SYNC_TO_CTE_ONLY (0x10, bit 4): Do not sync to packets without a Constant Tone Extension

Default: 0

Set the sync CTE type to limit what types of periodic advertisers to sync to when scanning for periodic advertising synchronization. The set parameter takes effect immediately for all advertisers that have not already established synchronization.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14157 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_set_default_sync_receive_parameters#

sl_status_t sl_bt_cte_receiver_set_default_sync_receive_parameters (uint8_t mode, uint16_t skip, uint16_t timeout, uint8_t sync_cte_type, uint8_t reporting_mode)
Parameters
[in]mode

Enum sl_bt_past_receiver_mode_t. The mode to specify how the Bluetooth stack reacts when synchronization information is received. Values:

  • sl_bt_past_receiver_mode_ignore (0x0): No attempt is made to synchronize to a periodic advertising train for which the synchronization information was received. No event will be triggered towards the application.

  • sl_bt_past_receiver_mode_synchronize (0x1): Attempt to synchronize to a periodic advertising train for which the synchronization information was received. When the information is received, an event will be triggered to indicate success or failure and to provide the application with the periodic advertising synchronization handle.

Default: sl_bt_past_receiver_mode_ignore (No attempt is made to synchronize)

[in]skip

The maximum number of periodic advertising packets that can be skipped after a successful receive.

  • Range: 0 to 499

  • Default : 0

[in]timeout

The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.

  • Range: 10 to 16384

  • Unit: 10 ms

  • Time range: 100 ms to 163.84 s

    • Default : 1000 ms

[in]sync_cte_type

Sync CTE type flags to limit what types of periodic advertising trains to sync to when receiving sync transfers. This value can be a bitmask of multiple flags from CTE type flags for limiting periodic advertising synchronization. Flags:

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOA (0x01, bit 0): Do not sync to packets with an AoA Constant Tone Extension

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_1_US (0x02, bit 1): Do not sync to packets with an AoD Constant Tone Extension with 1 us slots

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_2_US (0x04, bit 2): Do not sync to packets with an AoD Constant Tone Extension with 2 us slots

  • SL_BT_CTE_RECEIVER_SYNC_TO_CTE_ONLY (0x10, bit 4): Do not sync to packets without a Constant Tone Extension

Default: 0 (do not limit synchronization by CTE type)

[in]reporting_mode

Enum sl_bt_sync_reporting_mode_t. Specifies the initial mode for reporting data received in the periodic advertising train after it has achieved synchronization. Values:

  • sl_bt_sync_report_none (0x0): Data received in periodic advertising trains is not reported to the application.

  • sl_bt_sync_report_all (0x1): Data received in periodic advertising trains is reported to the application.

Default: sl_bt_sync_report_all (Data received in periodic advertising trains is reported to the application)

Set the default parameters and the CTE type limitation for receiving Periodic Advertising Synchronization Transfers (PAST) over connections. The default parameters will be in effect for all subsequent connections and do not affect connections that have already opened. The parameters can be overridden for a specific connection using command sl_bt_cte_receiver_set_sync_receive_parameters after the connection is opened.

Irrespective of the value of the skip parameter, the Controller stops skipping packets if the skipping would cause a timeout.

This command is relevant and available only when the application has included the bluetooth_feature_past_receiver component into the build. If the PAST receiver component is not included, this command returns the error SL_STATUS_NOT_AVAILABLE.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events

  • sl_bt_evt_periodic_sync_transfer_received - Triggered after synchronization transfer is received for a periodic advertising train that does not have subevents or response slots.

  • sl_bt_evt_pawr_sync_transfer_received - If the application includes the bluetooth_feature_pawr_sync component, triggered after synchronization transfer is received for a Periodic Advertising with Responses (PAwR) train.


Definition at line 14251 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_set_sync_receive_parameters#

sl_status_t sl_bt_cte_receiver_set_sync_receive_parameters (uint8_t connection, uint8_t mode, uint16_t skip, uint16_t timeout, uint8_t sync_cte_type, uint8_t reporting_mode)
Parameters
[in]connection

Connection handle

[in]mode

Enum sl_bt_past_receiver_mode_t. The mode to specify how the Bluetooth stack reacts when synchronization information is received. Values:

  • sl_bt_past_receiver_mode_ignore (0x0): No attempt is made to synchronize to a periodic advertising train for which the synchronization information was received. No event will be triggered towards the application.

  • sl_bt_past_receiver_mode_synchronize (0x1): Attempt to synchronize to a periodic advertising train for which the synchronization information was received. When the information is received, an event will be triggered to indicate success or failure and to provide the application with the periodic advertising synchronization handle.

Default: sl_bt_past_receiver_mode_ignore (Do not attempt to synchronize)

[in]skip

The maximum number of periodic advertising packets that can be skipped after a successful receive.

  • Range: 0 to 499

  • Default : 0

[in]timeout

The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.

  • Range: 10 to 16384

  • Unit: 10 ms

  • Time range: 100 ms to 163.84 s

  • Default : 1000 ms

[in]sync_cte_type

Sync CTE type flags to limit what types of periodic advertising trains to sync to when receiving sync transfers. This value can be a bitmask of multiple flags from CTE type flags for limiting periodic advertising synchronization. Flags:

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOA (0x01, bit 0): Do not sync to packets with an AoA Constant Tone Extension

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_1_US (0x02, bit 1): Do not sync to packets with an AoD Constant Tone Extension with 1 us slots

  • SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_2_US (0x04, bit 2): Do not sync to packets with an AoD Constant Tone Extension with 2 us slots

  • SL_BT_CTE_RECEIVER_SYNC_TO_CTE_ONLY (0x10, bit 4): Do not sync to packets without a Constant Tone Extension

Default: 0 (do not limit synchronization by CTE type)

[in]reporting_mode

Enum sl_bt_sync_reporting_mode_t. Specifies the initial mode for reporting data received in the periodic advertising train after it has achieved synchronization. Values:

  • sl_bt_sync_report_none (0x0): Data received in periodic advertising trains is not reported to the application.

  • sl_bt_sync_report_all (0x1): Data received in periodic advertising trains is reported to the application.

Default: sl_bt_sync_report_all (Data received in periodic advertising trains is reported to the application)

Set the parameters and the CTE type limitation for receiving Periodic Advertising Synchronization Transfers (PAST) over the specified connection. The parameters do not affect periodic advertising trains that the device has already synchronized to.

Irrespective of the value of the skip parameter, the Controller stops skipping packets if the skipping would cause a timeout.

This command is relevant and available only when the application has included the bluetooth_feature_past_receiver component into the build. If the PAST receiver component is not included, this command returns the error SL_STATUS_NOT_AVAILABLE.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events

  • sl_bt_evt_periodic_sync_transfer_received - Triggered after synchronization transfer is received for a periodic advertising train that does not have subevents or response slots.

  • sl_bt_evt_pawr_sync_transfer_received - If the application includes the bluetooth_feature_pawr_sync component, triggered after synchronization transfer is received for a Periodic Advertising with Responses (PAwR) train.


Definition at line 14347 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_configure#

sl_status_t sl_bt_cte_receiver_configure (uint8_t flags)
Parameters
N/Aflags

Definition at line 14374 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_enable_connection_cte#

sl_status_t sl_bt_cte_receiver_enable_connection_cte (uint8_t connection, uint16_t interval, uint8_t cte_length, uint8_t cte_type, uint8_t slot_durations, size_t switching_pattern_len, const uint8_t * switching_pattern)
Parameters
[in]connection

Connection handle

[in]interval

Measurement interval. CTE requests may be sent less often. For example, if a connection event is missed for any reason, the CTE request will be sent in the next connection event.

  • 0: No interval. The request is initiated only once.

  • Other values N: Initiate the request every N-th connection events

[in]cte_length

Minimum CTE length requested in 8 us units.

  • Range: 2 to 20

  • Time Range: 16 us to 160 us

[in]cte_type

Requested CTE type

  • 0: AoA CTE

  • 1: AoD CTE with 1 us slots

  • 2: AoD CTE with 2 us slots

[in]slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each

[in]switching_pattern_len

Length of data in switching_pattern

[in]switching_pattern

Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over.

Start IQ samplings on a connection. A CTE requests will be initiated periodically on the given connection and IQ sampling will be made on the received CTE responses.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 14414 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_disable_connection_cte#

sl_status_t sl_bt_cte_receiver_disable_connection_cte (uint8_t connection)
Parameters
[in]connection

Connection handle

Stop the IQ sampling on a connection. CTEs will not be requested on the given connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14432 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_enable_connectionless_cte#

sl_status_t sl_bt_cte_receiver_enable_connectionless_cte (uint16_t sync, uint8_t slot_durations, uint8_t cte_count, size_t switching_pattern_len, const uint8_t * switching_pattern)
Parameters
[in]sync

Periodic advertising synchronization handle

[in]slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each

[in]cte_count

- 0: Sample and report all available CTEs

  • Other values: Maximum number of sampled CTEs in each periodic advertising interval

[in]switching_pattern_len

Length of data in switching_pattern

[in]switching_pattern

Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over.

Start IQ sampling on a periodic advertising synchronization. IQ samples are taken on each CTE found in the periodic advertisements.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 14458 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_disable_connectionless_cte#

sl_status_t sl_bt_cte_receiver_disable_connectionless_cte (uint16_t sync)
Parameters
[in]sync

Periodic advertising synchronization handle

Stop IQ sampling on a periodic advertising synchronization.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14473 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_enable_silabs_cte#

sl_status_t sl_bt_cte_receiver_enable_silabs_cte (uint8_t slot_durations, uint8_t cte_count, size_t switching_pattern_len, const uint8_t * switching_pattern)
Parameters
[in]slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each

[in]cte_count

- 0: Sample and report all available CTEs

  • Other values: Maximum number of sampled CTEs in each extended advertising interval

[in]switching_pattern_len

Length of data in switching_pattern

[in]switching_pattern

Antenna switching pattern. Antennas will be switched in this order with the antenna switch pins during CTE. If the CTE is longer than the switching pattern, the pattern starts over.

Enable IQ sampling of Silicon Labs CTE found in extended advertisements.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 14497 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cte_receiver_disable_silabs_cte#

sl_status_t sl_bt_cte_receiver_disable_silabs_cte ()

Disable IQ sampling of Silicon Labs CTE.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14510 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h