User Messaging#

User Messaging.

This class provides commands and events, which can be used by a NCP host and target to implement a communication mechanism with a custom proprietary protocol. An application must decide whether and how the command and event are used. The Bluetooth host stack does not produce or consume any messages belonging to this class.

Modules#

sl_bt_evt_user_message_to_host

sl_bt_evt_user_cs_service_message_to_host

Functions#

sl_status_t
sl_bt_user_message_to_target(size_t data_len, const uint8_t *data, size_t max_response_size, size_t *response_len, uint8_t *response)
sl_status_t
sl_bt_user_manage_event_filter(size_t data_len, const uint8_t *data)
sl_status_t
sl_bt_user_cs_service_message_to_target(size_t data_len, const uint8_t *data, size_t max_response_size, size_t *response_len, uint8_t *response)

Macros#

#define
sl_bt_cmd_user_message_to_target_id 0x00ff0020
#define
sl_bt_cmd_user_manage_event_filter_id 0x01ff0020
#define
sl_bt_cmd_user_reset_to_dfu_id 0x02ff0020
#define
sl_bt_cmd_user_cs_service_message_to_target_id 0x03ff0020
#define
sl_bt_rsp_user_message_to_target_id 0x00ff0020
#define
sl_bt_rsp_user_manage_event_filter_id 0x01ff0020
#define
sl_bt_rsp_user_reset_to_dfu_id 0x02ff0020
#define
sl_bt_rsp_user_cs_service_message_to_target_id 0x03ff0020

Function Documentation#

sl_bt_user_message_to_target#

sl_status_t sl_bt_user_message_to_target (size_t data_len, const uint8_t * data, size_t max_response_size, size_t * response_len, uint8_t * response)
Parameters
[in]data_len

Length of data in data

[in]data

The message

[in]max_response_size

Size of output buffer passed in response

[out]response_len

On return, set to the length of output data written to response

[out]response

The response message

Used by an NCP host to send a message to the target application on device. The application on the target must send the response with sl_bt_send_rsp_user_message_to_target.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14780 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_user_manage_event_filter#

sl_status_t sl_bt_user_manage_event_filter (size_t data_len, const uint8_t * data)
Parameters
[in]data_len

Length of data in data

[in]data

The message for managing event filter

Manage NCP event filter. When the event filter is in use, API events passing the filter will be sent to the host and those that do not pass are discarded by the target. For functionality details, see the NCP component in the Bluetooth SDK.

By default, the NCP does not use the event filter.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14801 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_user_reset_to_dfu#

void sl_bt_user_reset_to_dfu ()

Reset the target device to DFU mode from the NCP host. This command is used by specific SDK DFU component on the target device for the functionality related to DFU. Do not use it in other circumstances. This command does not have a response.


Definition at line 14813 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_user_cs_service_message_to_target#

sl_status_t sl_bt_user_cs_service_message_to_target (size_t data_len, const uint8_t * data, size_t max_response_size, size_t * response_len, uint8_t * response)
Parameters
[in]data_len

Length of data in data

[in]data

The message

[in]max_response_size

Size of output buffer passed in response

[out]response_len

On return, set to the length of output data written to response

[out]response

The response message

Used by an NCP host to send a message to the Channel Sounding service component on target device. The Channel Sounding service on target device must send the response with sl_bt_send_rsp_user_cs_service_message_to_target.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 14832 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h