sl_bt_evt_user_message_to_host#

Used by the target application on a device to initiate communication and send a message to the NCP host.

Do not send event messages in the context of the user command handling.

Modules#

sl_bt_evt_user_message_to_host_s

Macros#

#define
sl_bt_evt_user_message_to_host_id 0x00ff00a0

Identifier of the message_to_host event.

Typedef Documentation#

sl_bt_evt_user_message_to_host_t#

typedef struct sl_bt_evt_user_message_to_host_s sl_bt_evt_user_message_to_host_t

Definition at line 14738 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h