sl_bt_evt_connection_data_length#

Reports a change to the maximum payload length or maximum TX time in either direction of a connection.

Modules#

sl_bt_evt_connection_data_length_s

Macros#

#define

Identifier of the data_length event.

Typedef Documentation#

sl_bt_evt_connection_data_length_t#

typedef struct sl_bt_evt_connection_data_length_s sl_bt_evt_connection_data_length_t

Definition at line 6263 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_data_length_id#

#define sl_bt_evt_connection_data_length_id
Value:
0x090600a0

Identifier of the data_length event.


Definition at line 6245 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h