sl_bt_evt_connection_remote_tx_power#
Reports a transmit power change of the connection on the remote device that supports the LE Power Control for the connection.
This event is enabled if reporting the remote transmit power change has been enabled with the sl_bt_connection_set_remote_power_reporting command.
Modules#
sl_bt_evt_connection_remote_tx_power_s
Typedefs#
Macros#
#define
sl_bt_evt_connection_remote_tx_power_id 0x070600a0
Identifier of the remote_tx_power event.
Typedef Documentation#
sl_bt_evt_connection_remote_tx_power_t#
typedef struct sl_bt_evt_connection_remote_tx_power_s sl_bt_evt_connection_remote_tx_power_t
Definition at line
6205
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_remote_tx_power_id#
#define sl_bt_evt_connection_remote_tx_power_idValue:
0x070600a0
Identifier of the remote_tx_power event.
Definition at line
6156
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h