sl_bt_evt_connection_remote_used_features#

List of link layer features supported by the remote device.

Modules#

sl_bt_evt_connection_remote_used_features_s

Macros#

#define

Identifier of the remote_used_features event.

Typedef Documentation#

sl_bt_evt_connection_remote_used_features_t#

typedef struct sl_bt_evt_connection_remote_used_features_s sl_bt_evt_connection_remote_used_features_t

Definition at line 6233 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_remote_used_features_id#

#define sl_bt_evt_connection_remote_used_features_id
Value:
0x080600a0

Identifier of the remote_used_features event.


Definition at line 6216 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h