BLE Peer Manager Common#
Peer Manager for Bluetooth Low Energy. Responsible for advertising and creating connections. The user can set the advertising parameters.
Modules#
Enumerations#
enum
BLE_PEER_MANAGER_ON_CONN_OPENED_CENTRAL = 0
BLE_PEER_MANAGER_ON_CONN_OPENED_PERIPHERAL 
BLE_PEER_MANAGER_ON_CONN_CLOSED 
BLE_PEER_MANAGER_ON_ADV_STOPPED 
BLE_PEER_MANAGER_ERROR 
}
Typedefs#
typedef struct ble_peer_manager_evt_type_s
Functions#
void
ble_peer_manager_on_event(ble_peer_manager_evt_type_t *event)
Macros#
#define
BLE_PEER_MANAGER_COMMON_LOG 0
#define
BLE_PEER_MANAGER_COMMON_LOG_PREFIX "[PM]"
#define
BLE_PEER_MANAGER_COMMON_MAX_ALLOWED_CONN_COUNT 4
#define
BLE_PEER_MANAGER_COMMON_TIMEOUT_GATT_MS 10000
Enumeration Documentation#
ble_peer_manager_evt_id#
ble_peer_manager_evt_id
| Enumerator | |
|---|---|
| BLE_PEER_MANAGER_ON_CONN_OPENED_CENTRAL | |
| BLE_PEER_MANAGER_ON_CONN_OPENED_PERIPHERAL | |
| BLE_PEER_MANAGER_ON_CONN_CLOSED | |
| BLE_PEER_MANAGER_ON_ADV_STOPPED | |
| BLE_PEER_MANAGER_ERROR | |
Typedef Documentation#
Function Documentation#
ble_peer_manager_on_event#
void ble_peer_manager_on_event (ble_peer_manager_evt_type_t * event)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| ble_peer_manager_evt_type_t * | N/A | event |