Power supply measurement#
Power supply measurement HW abstraction designed for development boards with coin cell battery support, i.e. Thunderboard and Dev Kit. Not suitable for other applications.
Functions#
Macros#
Unknown power supply type.
The board powered from the USB connector.
The board powered from AA batteries.
The board powered from AAA batteries.
The board powered from a CR2032 battery.
Function Documentation#
sl_power_supply_probe#
void sl_power_supply_probe (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Probe the connected supply and determine its type.
Note
- The results can be acquired with sl_power_supply_get_characteristics. 
sl_power_supply_get_characteristics#
void sl_power_supply_get_characteristics (uint8_t * type, float * voltage, float * ir)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | [out] | type | Supply type. | 
| float * | [out] | voltage | Supply voltage. | 
| float * | [out] | ir | Internal resistance of the supply. | 
Retrieve the supply characteristic variables.
sl_power_supply_get_type#
uint8_t sl_power_supply_get_type (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Getter for the power supply type.
Returns
- Power supply type represented as an integer. 
sl_power_supply_is_low_power#
bool sl_power_supply_is_low_power (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Checks if the current power supply has low power capability.
Returns
- True if the supply is low power type, false otherwise. 
sl_power_supply_measure_voltage#
float sl_power_supply_measure_voltage (unsigned int avg)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| unsigned int | [in] | avg | Number of measurements to average. | 
Measure the supply voltage by averaging multiple readings.
Returns
- The measured voltage. 
sl_power_supply_get_battery_level#
uint8_t sl_power_supply_get_battery_level (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Measure the battery level.
Returns
- The estimated battery capacity level in percent.