CS Initiator Display#
Prints Channel Sounding (CS) Initiator status information to the LCD of the WSTK.
Modules#
cs_initiator_display_content_t
Enumerations#
Display rows.
UI alignment.
Functions#
Macros#
Enumeration Documentation#
cs_initiator_display_row_t#
cs_initiator_display_row_t
Display rows.
| Enumerator | |
|---|---|
| ROW_SYSTEM | |
| ROW_ROLE | |
| ROW_MODE | |
| ROW_DISTANCE_TEXT | |
| ROW_DISTANCE_VALUE | |
| ROW_LIKELINESS_TEXT | |
| ROW_LIKELINESS_VALUE | |
| ROW_RSSI_DISTANCE_TEXT | |
| ROW_RSSI_DISTANCE_VALUE | |
| ROW_BIT_ERROR_RATE_TEXT | |
| ROW_BIT_ERROR_RATE_VALUE | |
| ROW_STATE | |
cs_initiator_display_alignment_t#
cs_initiator_display_alignment_t
UI alignment.
| Enumerator | |
|---|---|
| CS_INITIATOR_DISPLAY_ALIGNMENT_LEFT | |
| CS_INITIATOR_DISPLAY_ALIGNMENT_CENTER | |
| CS_INITIATOR_DISPLAY_ALIGNMENT_RIGHT | |
Function Documentation#
cs_initiator_display_set_distance#
void cs_initiator_display_set_distance (float distance)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | distance | Distance value | 
Set distance value to display
cs_initiator_display_set_distance_progress#
void cs_initiator_display_set_distance_progress (float progress_percentage)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | progress_percentage | Distance progress percentage | 
Set distance progress percentage to display
cs_initiator_display_set_rssi_distance#
void cs_initiator_display_set_rssi_distance (float distance)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | distance | RSSI distance value | 
Set RSSI based distance value to display
cs_initiator_display_set_likeliness#
void cs_initiator_display_set_likeliness (float likeliness)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | likeliness | likeliness value | 
Set the likeliness parameter to display
cs_initiator_display_set_bit_error_rate#
void cs_initiator_display_set_bit_error_rate (float ber)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | ber | BER value | 
Set the Bit Error Rate (BER) value to display
cs_initiator_display_set_measurement_mode#
void cs_initiator_display_set_measurement_mode (sl_bt_cs_mode_t mode, uint8_t algo_mode)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_cs_mode_t | [in] | mode | CS measurement mode. | 
| uint8_t | [in] | algo_mode | Object tracking mode. | 
Set the measurement mode and object tracking mode to display
cs_initiator_display_print_float_value#
void cs_initiator_display_print_float_value (float value, uint8_t row, char * unit)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| float | [in] | value | the calculated value | 
| uint8_t | [in] | row | number of the row to print on, see cs_initiator_display_row_t | 
| char * | [in] | unit | unit string, in case of NULL no unit displayed | 
Print floating point value on the LCD with an optional unit string.
cs_initiator_display_on_event#
void cs_initiator_display_on_event (sl_bt_msg_t * evt)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. | 
Bluetooth stack event handler.
cs_initiator_display_init#
sl_status_t cs_initiator_display_init (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Initialize the display.
cs_initiator_display_update#
void cs_initiator_display_update (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Update the display.
cs_initiator_display_set_alignment#
void cs_initiator_display_set_alignment (cs_initiator_display_alignment_t align)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| cs_initiator_display_alignment_t | [in] | align | text alignment to use | 
Set the display text alignment.
cs_initiator_display_write_text#
void cs_initiator_display_write_text (char * str, uint8_t row)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| char * | [in] | str | pointer to the text to print | 
| uint8_t | [in] | row | row to print the text on | 
Write text on the LCD.