ESL Tag User Defined Display Driver#
This component provides skeleton code for a user defined display driver - to be filled in with actual low level driver code for driving any arbitrary ESL Tag display type. See the Doxygen comments in the header file on usage. This is a Custom-Code component.
Functions#
Function Documentation#
esl_user_display_init#
sl_status_t esl_user_display_init (int param_count, ... )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| int | [in] | param_count | Number of parameters following (mandatory, equals to 'ESL_DISPLAY_INIT_FUNC_PARAMETERS_COUNT' defined by esl_tag_display component. | 
| ... | [in] | uint8_t type of the display index | 
ESL Tag user defined display driver init function. Function naming is for reference, only - any arbitrary function naming can be used, freely. For more - and especially, different type of displays - there might be a good approach to implement more init functions, also. Then, these functions has to be assigned to the corresponding display during the esl_core_boot_event as follows:
sl_status_t void esl_core_boot_event(void)
{
 sl_status_t sc;
 esl_display_info_p info;
 sc = esl_display_create(<user_display_witdth>,
                         <user_display_height>,
                         <user_display_type>,
                         &info);
 app_assert_status(sc);
 sc = esl_display_add(info,
                      <your_init_function>,      // can be NULL if not needed
                      <your_write_function>);    // mandatory!
 app_assert_status(sc);
}
Note: please do not forget to add #include "esl_display.h", previously.
esl_user_display_write#
sl_status_t esl_user_display_write (int param_count, ... , image_index)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| int | [in] | param_count | Number of parameters following (mandatory, equals to 'ESL_DISPLAY_WRITE_FUNC_PARAMETERS_COUNT' defined by esl_tag_display component. | 
| ... | [in] | uint8_t type of the display index | |
| [in] | image_index | uint8_t type of the image index | 
ESL Tag display user defined driver write function. See the comments at esl_user_display_init function on naming and usage.