Data structure of the channel_classification event.

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_connection_channel_classification_s::connection

Connection handle


classification_map#

sl_bt_channel_classification_map_t sl_bt_evt_connection_channel_classification_s::classification_map

A fixed-length byte array of 10 bytes consisting of 40 2-bit fields.

Only the first 37 fields are used by channel classification. The nth field (numbering from 0) contains the classification value of data channel index n. Classification is defined as following values:

  • Value 0: Unknown

  • Value 1: Good

  • Value 3: Bad