Data structure of the data_length event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_data_length_s::connection
Connection handle
Definition at line
5944
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
tx_data_len#
uint16_t sl_bt_evt_connection_data_length_s::tx_data_len
The maximum payload octets of a packet that the local Controller will send
Definition at line
5945
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
tx_time_us#
uint16_t sl_bt_evt_connection_data_length_s::tx_time_us
The maximum time in microseconds that the local Controller will take to send a data packet
Definition at line
5947
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
rx_data_len#
uint16_t sl_bt_evt_connection_data_length_s::rx_data_len
The maximum payload octets of a packet that the local Controller expects to receive
Definition at line
5949
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
rx_time_us#
uint16_t sl_bt_evt_connection_data_length_s::rx_time_us
The maximum time in microseconds that the local Controller expects to take to receive a data packet
Definition at line
5951
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h