sl_bt_evt_periodic_advertiser_status#
This event reports the latest status of periodic advertising on an advertising set.
It is generated for each scheduled periodic advertising transmission when the status report has been enabled. By default, this event is disabled in the Bluetooth stack. Use command sl_bt_system_linklayer_configure and key sl_bt_system_linklayer_config_key_set_periodic_advertising_status_report to enable or disable it.
Modules#
sl_bt_evt_periodic_advertiser_status_s
Typedefs#
Macros#
#define
sl_bt_evt_periodic_advertiser_status_id 0x005800a0
Identifier of the status event.
Typedef Documentation#
sl_bt_evt_periodic_advertiser_status_t#
typedef struct sl_bt_evt_periodic_advertiser_status_s sl_bt_evt_periodic_advertiser_status_t
Definition at line
3274
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_periodic_advertiser_status_id#
#define sl_bt_evt_periodic_advertiser_status_idValue:
0x005800a0
Identifier of the status event.
Definition at line
3255
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h