Data structure of the key_refresh_phase_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
netkey_index#
uint16_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::netkey_index
Network key index for which the state applies
value#
uint8_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::value
Key refresh phase state of the node for the given network key. Valid values are:
- 0: Normal operation 
- 1: First phase of key refresh procedure 
- 2: Second phase of key refresh procedure