You are viewing documentation for version:
Data structure of the upload_failed event. 
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_failed_s::elem_index
Server model element index 
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_failed_s::client_address
Address of the Distribution Client 
size#
uint32_t sl_btmesh_evt_fw_dist_server_upload_failed_s::size
Upload size 
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_server_upload_failed_s::blob_id
BLOB ID 
fwid#
uint8array sl_btmesh_evt_fw_dist_server_upload_failed_s::fwid
FWID of the firmware image