Data structure of the unprov_beacon event.
Public Attribute Documentation#
oob_capabilities#
uint16_t sl_btmesh_evt_prov_unprov_beacon_s::oob_capabilities
OOB capabilities bitfield, which indicates the means by which out-of-band provisioning data may be retrieved. See OOB Capabilities.
uri_hash#
uint32_t sl_btmesh_evt_prov_unprov_beacon_s::uri_hash
Hash of the out-of-band URI, which is received in sl_btmesh_evt_prov_uri. If the URI bit (bit 1) is not set in the OOB capabilities bitfield, this field is ignored.
bearer#
uint8_t sl_btmesh_evt_prov_unprov_beacon_s::bearer
Bearer on which the beacon was seen. Values are as follows:
- 0: PB-ADV 
- 1: PB-GATT 
address_type#
uint8_t sl_btmesh_evt_prov_unprov_beacon_s::address_type
Beaconing device address type. Values:
- 0: Public address 
- 1: Random address