Data structure of the register_get event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_scene_server_register_get_s::destination_address
Address of the server or the group address to which it was published.
elem_index#
uint16_t sl_btmesh_evt_scene_server_register_get_s::elem_index
Index of the element which received the command.
client_address#
uint16_t sl_btmesh_evt_scene_server_register_get_s::client_address
Device which sent the request.
appkey_index#
uint16_t sl_btmesh_evt_scene_server_register_get_s::appkey_index
Appkey used by client_address.