Configuration

User-configurable stack configuration macros and defaults. More...

Macros

#define EMBER_HEAP_SIZE 2000
The size in bytes of the Ember heap. See Memory_buffer for more details. More...
#define EMBER_CHILD_TABLE_SIZE 0
The maximum number of children supported by the device. Can be configured from 0 to 64. 11B of token space is allocated for each child in the table. More...
#define EMBER_CHILD_TABLE_TOKEN_SIZE EMBER_CHILD_TABLE_SIZE
#define EMBER_CHILD_TIMEOUT_SEC 3600
Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent may remove the child from the child table. In particular the parent shall remove the oldest stale child whenever the child table is full and there is the need of making room for a new child. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use emberPollForData() as keep alive mechanism, or use the Poll plugin. The maximum allowed timeout value is EMBER_CHILD_TABLE_MAX_TIMEOUT_S . Setting the timeout value to EMBER_CHILD_TABLE_AGING_DISABLED disables aging of the child table. More...
#define EMBER_INDIRECT_QUEUE_SIZE 0
Indirect queue is used on a parent to store a message intended for a sleepy end device, this configures the size of that queue. Configure it to 0 if parent support plugin is not used. More...
#define EMBER_MAC_OUTGOING_QUEUE_SIZE 0
MAC Outgoing paclet queue is to store messages until the radio is available to send it (In most cases, the radio is unavailable because it's already transmitting). The configures the size of that queue. More...
#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS 8000
The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child. The maximum value is 30 seconds (30000 milliseconds). More...
#define EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC 60
The period in seconds a range extender sends an update command to the coordinator containing the list of its children. More...
#define EMBER_MAC_ACK_TIMEOUT_MS 25
The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used. The maximum allowed value is 65. More...
#define EMBER_RADIO_CCA_THRESHOLD -65
The CCA threshold used at the MAC layer for CSMA/CA, in dBm. More...
#define EMBER_FREQUENCY_HOPPING_SEED 0
The frequency hopping channel sequence generation seed. Can be configured between 0 and 65535. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_START_CHANNEL 0
The lowest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_END_CHANNEL 24
The highest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS 400
The time in milliseconds to stay on each channel for frequency hopping. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS 20
The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S 15
The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S 60
The duration in seconds after which a sleepy client should resync with the server if the last resync happened more than this duration ago. See the Frequency Hopping chapter of UG235.03 for more details. More...
#define EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S (100)
The maximum duration in seconds a non sleepy client would keep hopping without receiving frequency hopping information from the server, after which the synchronization with the server is deemed lost. A special value of EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_DISABLE_TIMEOUT disables this timeout. More...
#define EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT (3)
When a node is started a frequency hopping server, it will first advertise on all channels to resynchronize all existing clients in case the server was started as result of a reboot. This parameter defines the number of iterations over the entire hopping sequence. More...
#define EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED 1
An EMBER_STAR_COORDINATOR assigns short IDs to other nodes in the star network sequentially starting from this short ID. This option provides a simple effective way to reserve an pool of short addresses for commissioning. More...
#define EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE 10
The size of the short-to-long address mapping table. See emberMacAddShortToLongAddressMapping for more details. More...

Detailed Description

User-configurable stack configuration macros and defaults.

Connect stack provides various interfaces to apply configuration:

  • APIs to change configuration run-time
  • Manufacturing tokens to change configuration during device flashing
  • Macros to change configuration at compile-time

The compile time configuration macros and their default values are listed here.

The default values are always chosen to make it usable for most applications, but in some cases, you might need to change it. The recommended way is to either define the macro you need to change in the compilation command (e.g. gcc -D) or you by manipulating the configuration options in the configurator GUI.

See ember-configuration-defaults.h for source code.

Macro Definition Documentation

◆ EMBER_CHILD_TABLE_SIZE

#define EMBER_CHILD_TABLE_SIZE 0

The maximum number of children supported by the device. Can be configured from 0 to 64. 11B of token space is allocated for each child in the table.

Note
It's recommended to set it to 64 for EMBER_STAR_COORDINATOR , 32 for EMBER_STAR_RANGE_EXTENDER and 0 for anything else.
Warning
This should be configured from the Parent Support plugin options.

Definition at line 102 of file ember-configuration-defaults.h .

◆ EMBER_CHILD_TABLE_TOKEN_SIZE

#define EMBER_CHILD_TABLE_TOKEN_SIZE EMBER_CHILD_TABLE_SIZE

Definition at line 105 of file ember-configuration-defaults.h .

◆ EMBER_CHILD_TIMEOUT_SEC

#define EMBER_CHILD_TIMEOUT_SEC 3600

Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent may remove the child from the child table. In particular the parent shall remove the oldest stale child whenever the child table is full and there is the need of making room for a new child. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use emberPollForData() as keep alive mechanism, or use the Poll plugin. The maximum allowed timeout value is EMBER_CHILD_TABLE_MAX_TIMEOUT_S . Setting the timeout value to EMBER_CHILD_TABLE_AGING_DISABLED disables aging of the child table.

Warning
This should be configured from the Parent Support plugin options.

Definition at line 123 of file ember-configuration-defaults.h .

◆ EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED

#define EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED 1

An EMBER_STAR_COORDINATOR assigns short IDs to other nodes in the star network sequentially starting from this short ID. This option provides a simple effective way to reserve an pool of short addresses for commissioning.

Definition at line 276 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S

#define EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S (100)

The maximum duration in seconds a non sleepy client would keep hopping without receiving frequency hopping information from the server, after which the synchronization with the server is deemed lost. A special value of EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_DISABLE_TIMEOUT disables this timeout.

Definition at line 256 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS

#define EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS 400

The time in milliseconds to stay on each channel for frequency hopping. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 218 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS

#define EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS 20

The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 227 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_END_CHANNEL

#define EMBER_FREQUENCY_HOPPING_END_CHANNEL 24

The highest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 210 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_SEED

#define EMBER_FREQUENCY_HOPPING_SEED 0

The frequency hopping channel sequence generation seed. Can be configured between 0 and 65535. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 194 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT

#define EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT (3)

When a node is started a frequency hopping server, it will first advertise on all channels to resynchronize all existing clients in case the server was started as result of a reboot. This parameter defines the number of iterations over the entire hopping sequence.

Definition at line 266 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S

#define EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S 15

The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 236 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S

#define EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S 60

The duration in seconds after which a sleepy client should resync with the server if the last resync happened more than this duration ago. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 245 of file ember-configuration-defaults.h .

◆ EMBER_FREQUENCY_HOPPING_START_CHANNEL

#define EMBER_FREQUENCY_HOPPING_START_CHANNEL 0

The lowest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.

Definition at line 202 of file ember-configuration-defaults.h .

◆ EMBER_HEAP_SIZE

#define EMBER_HEAP_SIZE 2000

The size in bytes of the Ember heap. See Memory_buffer for more details.

Warning
This should be configured from the Parent Support plugin options.

Definition at line 90 of file ember-configuration-defaults.h .

◆ EMBER_INDIRECT_QUEUE_SIZE

#define EMBER_INDIRECT_QUEUE_SIZE 0

Indirect queue is used on a parent to store a message intended for a sleepy end device, this configures the size of that queue. Configure it to 0 if parent support plugin is not used.

Warning
This should be configured from the Parent Support plugin options.

Definition at line 139 of file ember-configuration-defaults.h .

◆ EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS

#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS 8000

The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child. The maximum value is 30 seconds (30000 milliseconds).

Warning
This should be configured from the Parent Support plugin options.

Definition at line 159 of file ember-configuration-defaults.h .

◆ EMBER_MAC_ACK_TIMEOUT_MS

#define EMBER_MAC_ACK_TIMEOUT_MS 25

The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used. The maximum allowed value is 65.

Definition at line 177 of file ember-configuration-defaults.h .

◆ EMBER_MAC_OUTGOING_QUEUE_SIZE

#define EMBER_MAC_OUTGOING_QUEUE_SIZE 0

MAC Outgoing paclet queue is to store messages until the radio is available to send it (In most cases, the radio is unavailable because it's already transmitting). The configures the size of that queue.

Warning
This should be configured from the MAC Packet Queue plugin options.

Definition at line 149 of file ember-configuration-defaults.h .

◆ EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC

#define EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC 60

The period in seconds a range extender sends an update command to the coordinator containing the list of its children.

Attention
This option is only used on EMBER_STAR_RANGE_EXTENDER device.

Definition at line 168 of file ember-configuration-defaults.h .

◆ EMBER_RADIO_CCA_THRESHOLD

#define EMBER_RADIO_CCA_THRESHOLD -65

The CCA threshold used at the MAC layer for CSMA/CA, in dBm.

Warning
This should be configured from the Connect Stack plugin options.

Definition at line 185 of file ember-configuration-defaults.h .

◆ EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE

#define EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE 10

The size of the short-to-long address mapping table. See emberMacAddShortToLongAddressMapping for more details.

Attention
This table is only used for EMBER_MAC_MODE_DEVICE and EMBER_MAC_MODE_SLEEPY_DEVICE , but the memory will be allocated on all device types.

Definition at line 287 of file ember-configuration-defaults.h .