tokTypeStackNodeData Struct Reference
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token. More...
#include <
token-stack.h
>
Data Fields | |
uint16_t | panId |
int16_t | radioTxPower |
uint16_t | radioFreqChannel |
uint8_t | nodeType |
uint16_t | nodeId |
uint16_t | parentId |
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token.
Definition at line 244
of file token-stack.h
.
Field Documentation
◆ nodeId
uint16_t tokTypeStackNodeData::nodeId |
The NodeId (short address) of the device
Definition at line 249
of file token-stack.h
.
◆ nodeType
uint8_t tokTypeStackNodeData::nodeType |
The EmberNodeType configured for the device
Definition at line 248
of file token-stack.h
.
◆ panId
uint16_t tokTypeStackNodeData::panId |
The PanId of the device
Definition at line 245
of file token-stack.h
.
◆ parentId
uint16_t tokTypeStackNodeData::parentId |
The NodeId of the device's parent, if any
Definition at line 250
of file token-stack.h
.
◆ radioFreqChannel
uint16_t tokTypeStackNodeData::radioFreqChannel |
The radio channel configured for the device
Definition at line 247
of file token-stack.h
.
◆ radioTxPower
int16_t tokTypeStackNodeData::radioTxPower |
The TX power configured for the device in deci-dBm
Definition at line 246
of file token-stack.h
.
The documentation for this struct was generated from the following file:
token-stack.h