Platform_common

Compiler and Platform specific definitions and typedefs common to all platforms. More...

Macros

#define MEMSET (d, v, l) memset(d, v, l)
Friendly convenience macro pointing to the C Stdlib functions. More...
#define MEMCOPY (d, s, l) memcpy(d, s, l)
#define MEMMOVE (d, s, l) memmove(d, s, l)
#define MEMPGMCOPY (d, s, l) memcpy(d, s, l)
#define MEMCOMPARE (s0, s1, l) memcmp(s0, s1, l)
#define MEMPGMCOMPARE (s0, s1, l) memcmp(s0, s1, l)

Generic Types

#define TRUE 1
An alias for one, used for clarity. More...
#define FALSE 0
An alias for zero, used for clarity. More...
#define NULL ((void *)0)
The null pointer. More...

Bit Manipulation Macros

#define BIT (x) (1U << (x))
Useful to reference a single bit of a byte. More...
#define BIT32 (x) (((uint32_t) 1) << (x))
Useful to reference a single bit of an uint32_t type. More...
#define SETBIT (reg, bit) (reg) |= BIT (bit)
Sets bit in the reg register or byte. More...
#define SETBITS (reg, bits) (reg) |= (bits)
Sets the bits in the reg register or the byte as specified in the bitmask bits . More...
#define CLEARBIT (reg, bit) (reg) &= ~( BIT (bit))
Clears a bit in the reg register or byte. More...
#define CLEARBITS (reg, bits) (reg) &= ~(bits)
Clears the bits in the reg register or byte as specified in the bitmask bits . More...
#define READBIT (reg, bit) ((reg) & ( BIT (bit)))
Returns the value of bit within the register or byte reg . More...
#define READBITS (reg, bits) ((reg) & (bits))
Returns the value of the bitmask bits within the register or byte reg . More...

Byte Manipulation Macros

#define LOW_BYTE (n) ((uint8_t)(n))
Returns the low byte of the 16-bit value n as an uint8_t . More...
#define HIGH_BYTE (n) LOW_BYTE ((n) >> 8)
Returns the high byte of the 16-bit value n as an uint8_t . More...
#define HIGH_LOW_TO_INT (high, low)
Returns the value built from the two uint8_t values high and low . More...
#define INT8U_TO_INT32U (byte3, byte2, byte1, byte0)
Returns the value built from the four uint8_t as an uint32_t . More...
#define BYTE_0 (n) ((uint8_t)(n))
Returns the low byte of the 32-bit value n as an uint8_t . More...
#define BYTE_1 (n) BYTE_0 ((n) >> 8)
Returns the second byte of the 32-bit value n as an uint8_t . More...
#define BYTE_2 (n) BYTE_0 ((n) >> 16)
Returns the third byte of the 32-bit value n as an uint8_t . More...
#define BYTE_3 (n) BYTE_0 ((n) >> 24)
Returns the high byte of the 32-bit value n as an uint8_t . More...
#define BYTE_4 (n) BYTE_0 ((n) >> 32)
Returns the fifth byte of the 64-bit value n as an uint8_t . More...
#define BYTE_5 (n) BYTE_0 ((n) >> 40)
Returns the sixth byte of the 64-bit value n as an uint8_t . More...
#define BYTE_6 (n) BYTE_0 ((n) >> 48)
Returns the seventh byte of the 64-bit value n as an uint8_t . More...
#define BYTE_7 (n) BYTE_0 ((n) >> 56)
Returns the high byte of the 64-bit value n as an uint8_t . More...
#define COUNTOF (a) (sizeof(a) / sizeof(a[0]))
Returns the number of entries in an array. More...

Time Manipulation Macros

#define elapsedTimeInt8u (oldTime, newTime) ((uint8_t) ((uint8_t)(newTime) - (uint8_t)(oldTime)))
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define elapsedTimeInt16u (oldTime, newTime) ((uint16_t) ((uint16_t)(newTime) - (uint16_t)(oldTime)))
Returns the elapsed time between two 16 bit values. Result may not be valid if the time samples differ by more than 32767. More...
#define elapsedTimeInt32u (oldTime, newTime) ((uint32_t) ((uint32_t)(newTime) - (uint32_t)(oldTime)))
Returns the elapsed time between two 32 bit values. Result may not be valid if the time samples differ by more than 2147483647. More...
#define MAX_INT8U_VALUE (0xFF)
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong. More...
#define HALF_MAX_INT8U_VALUE (0x80)
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define timeGTorEqualInt8u (t1, t2) ( elapsedTimeInt8u (t2, t1) <= ( HALF_MAX_INT8U_VALUE ))
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define MAX_INT16U_VALUE (0xFFFF)
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong. More...
#define HALF_MAX_INT16U_VALUE (0x8000)
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define timeGTorEqualInt16u (t1, t2) ( elapsedTimeInt16u (t2, t1) <= ( HALF_MAX_INT16U_VALUE ))
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define MAX_INT32U_VALUE (0xFFFFFFFFUL)
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong. More...
#define HALF_MAX_INT32U_VALUE (0x80000000UL)
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...
#define timeGTorEqualInt32u (t1, t2) ( elapsedTimeInt32u (t2, t1) <= ( HALF_MAX_INT32U_VALUE ))
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127. More...

Miscellaneous Macros

#define UNUSED_VAR (x) (void)(x)
#define DEBUG_LEVEL BASIC_DEBUG
Set debug level based on whether DEBUG or DEBUG_STRIPPED are defined. More...
#define STATIC_ASSERT (__condition, __errorstr)
Disable static assertions on compilers that don't support them. More...

Detailed Description

Compiler and Platform specific definitions and typedefs common to all platforms.

platform-common.h provides PLATFORM_HEADER defaults and common definitions. This head should never be included directly, it should only be included by the specific PLATFORM_HEADER used by your platform.

See platform-common.h for source code.

Macro Definition Documentation

◆ BIT

#define BIT ( x ) (1U << (x))

Useful to reference a single bit of a byte.

Definition at line 234 of file platform-common.h .

◆ BIT32

#define BIT32 ( x ) (((uint32_t) 1) << (x))

Useful to reference a single bit of an uint32_t type.

Definition at line 239 of file platform-common.h .

◆ BYTE_0

#define BYTE_0 ( n ) ((uint8_t)(n))

Returns the low byte of the 32-bit value n as an uint8_t .

Definition at line 321 of file platform-common.h .

◆ BYTE_1

#define BYTE_1 ( n ) BYTE_0 ((n) >> 8)

Returns the second byte of the 32-bit value n as an uint8_t .

Definition at line 326 of file platform-common.h .

◆ BYTE_2

#define BYTE_2 ( n ) BYTE_0 ((n) >> 16)

Returns the third byte of the 32-bit value n as an uint8_t .

Definition at line 331 of file platform-common.h .

◆ BYTE_3

#define BYTE_3 ( n ) BYTE_0 ((n) >> 24)

Returns the high byte of the 32-bit value n as an uint8_t .

Definition at line 336 of file platform-common.h .

◆ BYTE_4

#define BYTE_4 ( n ) BYTE_0 ((n) >> 32)

Returns the fifth byte of the 64-bit value n as an uint8_t .

Definition at line 341 of file platform-common.h .

◆ BYTE_5

#define BYTE_5 ( n ) BYTE_0 ((n) >> 40)

Returns the sixth byte of the 64-bit value n as an uint8_t .

Definition at line 346 of file platform-common.h .

◆ BYTE_6

#define BYTE_6 ( n ) BYTE_0 ((n) >> 48)

Returns the seventh byte of the 64-bit value n as an uint8_t .

Definition at line 351 of file platform-common.h .

◆ BYTE_7

#define BYTE_7 ( n ) BYTE_0 ((n) >> 56)

Returns the high byte of the 64-bit value n as an uint8_t .

Definition at line 356 of file platform-common.h .

◆ CLEARBIT

#define CLEARBIT ( reg,
bit
) (reg) &= ~( BIT (bit))

Clears a bit in the reg register or byte.

Note
Assuming reg is an IO register, some platforms (such as the AVR) can implement this in a single atomic operation.

Definition at line 260 of file platform-common.h .

◆ CLEARBITS

#define CLEARBITS ( reg,
bits
) (reg) &= ~(bits)

Clears the bits in the reg register or byte as specified in the bitmask bits .

Note
This is never a single atomic operation.

Definition at line 267 of file platform-common.h .

◆ COUNTOF

#define COUNTOF ( a ) (sizeof(a) / sizeof(a[0]))

Returns the number of entries in an array.

Definition at line 361 of file platform-common.h .

◆ DEBUG_LEVEL

#define DEBUG_LEVEL BASIC_DEBUG

Set debug level based on whether DEBUG or DEBUG_STRIPPED are defined.

Definition at line 457 of file platform-common.h .

◆ elapsedTimeInt16u

#define elapsedTimeInt16u ( oldTime,
newTime
) ((uint16_t) ((uint16_t)(newTime) - (uint16_t)(oldTime)))

Returns the elapsed time between two 16 bit values. Result may not be valid if the time samples differ by more than 32767.

Definition at line 383 of file platform-common.h .

◆ elapsedTimeInt32u

#define elapsedTimeInt32u ( oldTime,
newTime
) ((uint32_t) ((uint32_t)(newTime) - (uint32_t)(oldTime)))

Returns the elapsed time between two 32 bit values. Result may not be valid if the time samples differ by more than 2147483647.

Definition at line 390 of file platform-common.h .

◆ elapsedTimeInt8u

#define elapsedTimeInt8u ( oldTime,
newTime
) ((uint8_t) ((uint8_t)(newTime) - (uint8_t)(oldTime)))

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 376 of file platform-common.h .

◆ FALSE

#define FALSE 0

An alias for zero, used for clarity.

Definition at line 214 of file platform-common.h .

◆ HALF_MAX_INT16U_VALUE

#define HALF_MAX_INT16U_VALUE (0x8000)

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 407 of file platform-common.h .

◆ HALF_MAX_INT32U_VALUE

#define HALF_MAX_INT32U_VALUE (0x80000000UL)

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 416 of file platform-common.h .

◆ HALF_MAX_INT8U_VALUE

#define HALF_MAX_INT8U_VALUE (0x80)

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 398 of file platform-common.h .

◆ HIGH_BYTE

#define HIGH_BYTE ( n ) LOW_BYTE ((n) >> 8)

Returns the high byte of the 16-bit value n as an uint8_t .

Definition at line 297 of file platform-common.h .

◆ HIGH_LOW_TO_INT

#define HIGH_LOW_TO_INT ( high,
low
)
Value:
( \
((uint16_t) (((uint16_t) (high)) << 8)) \
+ ((uint16_t) ((low) & 0xFFu)) \
)

Returns the value built from the two uint8_t values high and low .

Definition at line 303 of file platform-common.h .

◆ INT8U_TO_INT32U

#define INT8U_TO_INT32U ( byte3,
byte2,
byte1,
byte0
)
Value:
( \
(((uint32_t) (byte3)) << 24) \
+ (((uint32_t) (byte2)) << 16) \
+ (((uint32_t) (byte1)) << 8) \
+ ((uint32_t) ((byte0) & 0xFFu)) \
)

Returns the value built from the four uint8_t as an uint32_t .

Definition at line 311 of file platform-common.h .

◆ LOW_BYTE

#define LOW_BYTE ( n ) ((uint8_t)(n))

Returns the low byte of the 16-bit value n as an uint8_t .

Definition at line 292 of file platform-common.h .

◆ MAX_INT16U_VALUE

#define MAX_INT16U_VALUE (0xFFFF)

Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.

Definition at line 406 of file platform-common.h .

◆ MAX_INT32U_VALUE

#define MAX_INT32U_VALUE (0xFFFFFFFFUL)

Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.

Definition at line 415 of file platform-common.h .

◆ MAX_INT8U_VALUE

#define MAX_INT8U_VALUE (0xFF)

Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.

Definition at line 397 of file platform-common.h .

◆ MEMCOMPARE

#define MEMCOMPARE ( s0,
s1,
l
) memcmp(s0, s1, l)

Definition at line 191 of file platform-common.h .

◆ MEMCOPY

#define MEMCOPY ( d,
s,
l
) memcpy(d, s, l)

Definition at line 188 of file platform-common.h .

◆ MEMMOVE

#define MEMMOVE ( d,
s,
l
) memmove(d, s, l)

Definition at line 189 of file platform-common.h .

◆ MEMPGMCOMPARE

#define MEMPGMCOMPARE ( s0,
s1,
l
) memcmp(s0, s1, l)

Definition at line 192 of file platform-common.h .

◆ MEMPGMCOPY

#define MEMPGMCOPY ( d,
s,
l
) memcpy(d, s, l)

Definition at line 190 of file platform-common.h .

◆ MEMSET

#define MEMSET ( d,
v,
l
) memset(d, v, l)

Friendly convenience macro pointing to the C Stdlib functions.

Definition at line 187 of file platform-common.h .

◆ NULL

#define NULL ((void *)0)

The null pointer.

Definition at line 221 of file platform-common.h .

◆ READBIT

#define READBIT ( reg,
bit
) ((reg) & ( BIT (bit)))

Returns the value of bit within the register or byte reg .

Definition at line 272 of file platform-common.h .

◆ READBITS

#define READBITS ( reg,
bits
) ((reg) & (bits))

Returns the value of the bitmask bits within the register or byte reg .

Definition at line 278 of file platform-common.h .

◆ SETBIT

#define SETBIT ( reg,
bit
) (reg) |= BIT (bit)

Sets bit in the reg register or byte.

Note
Assuming reg is an IO register, some platforms (such as the AVR) can implement this in a single atomic operation.

Definition at line 246 of file platform-common.h .

◆ SETBITS

#define SETBITS ( reg,
bits
) (reg) |= (bits)

Sets the bits in the reg register or the byte as specified in the bitmask bits .

Note
This is never a single atomic operation.

Definition at line 253 of file platform-common.h .

◆ STATIC_ASSERT

#define STATIC_ASSERT ( __condition,
__errorstr
)

Disable static assertions on compilers that don't support them.

Definition at line 465 of file platform-common.h .

◆ timeGTorEqualInt16u

#define timeGTorEqualInt16u ( t1,
t2
) ( elapsedTimeInt16u (t2, t1) <= ( HALF_MAX_INT16U_VALUE ))

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 408 of file platform-common.h .

◆ timeGTorEqualInt32u

#define timeGTorEqualInt32u ( t1,
t2
) ( elapsedTimeInt32u (t2, t1) <= ( HALF_MAX_INT32U_VALUE ))

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 417 of file platform-common.h .

◆ timeGTorEqualInt8u

#define timeGTorEqualInt8u ( t1,
t2
) ( elapsedTimeInt8u (t2, t1) <= ( HALF_MAX_INT8U_VALUE ))

Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.

Definition at line 399 of file platform-common.h .

◆ TRUE

#define TRUE 1

An alias for one, used for clarity.

Definition at line 209 of file platform-common.h .

◆ UNUSED_VAR

#define UNUSED_VAR ( x ) (void)(x)
Description:
Useful macro for avoiding compiler warnings related to unused function arguments or unused variables.

Definition at line 435 of file platform-common.h .