EmberTaskControl Struct Reference
Control structure for tasks. More...
#include <
ember-types.h
>
Data Fields |
|
uint32_t | nextEventTime |
EmberEventData * | events |
bool | busy |
Control structure for tasks.
This structure should not be accessed directly.
Definition at line
608
of file
ember-types.h
.
Field Documentation
◆ busy
bool EmberTaskControl::busy |
A flag that indicates the task has something to do other than events
Definition at line
614
of file
ember-types.h
.
◆ events
EmberEventData * EmberTaskControl::events |
The list of events associated with this task
Definition at line
612
of file
ember-types.h
.
◆ nextEventTime
uint32_t EmberTaskControl::nextEventTime |
The time when the next event associated with this task will fire
Definition at line
610
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h