Battery Monitor Callbacks#

These callbacks are contributed by the Battery Monitor plugin.

Functions#

void
emberAfPluginBatteryMonitorDataReadyCallback(uint16_t batteryVoltageMilliV)

Data Ready.

Function Documentation#

emberAfPluginBatteryMonitorDataReadyCallback#

void emberAfPluginBatteryMonitorDataReadyCallback (uint16_t batteryVoltageMilliV)

Data Ready.

Parameters
N/AbatteryVoltageMilliV

The battery voltage, in milli Volts Ver.: always

This function is called whenever the battery monitor has generated a new valid battery level.


Definition at line 97 of file ./app/ncp/doc/callback.doc