Multi-Network Stub Library Callbacks#

These callbacks are contributed by the Multi-Network Stub Library plugin.

Functions#

void
emberZigbeeKeyEstablishmentHandler(EmberEUI64 partner, EmberKeyStatus status)

Notifies the application of the status of the request for a Link Key. The application should define EMBER_APPLICATION_HAS_ZIGBEE_KEY_ESTABLISHMENT_HANDLER to implement its own handler.

Function Documentation#

emberZigbeeKeyEstablishmentHandler#

void emberZigbeeKeyEstablishmentHandler (EmberEUI64 partner, EmberKeyStatus status)

Notifies the application of the status of the request for a Link Key. The application should define EMBER_APPLICATION_HAS_ZIGBEE_KEY_ESTABLISHMENT_HANDLER to implement its own handler.

Parameters
N/Apartner

The IEEE address of the partner device or all zeros if the Key establishment failed.

N/Astatus

The status of the key establishment.


Definition at line 716 of file ./app/ncp/doc/callback.doc