Type describing the attribute default, min and max values.
This struct is required if the attribute mask specifies that this attribute has a known min and max values.
Public Attributes#
Public Attribute Documentation#
defaultValue#
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::defaultValue
Default value of the attribute.
Definition at line
113
of file ./app/framework/include/af-types.h
minValue#
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::minValue
Minimum allowed value
Definition at line
117
of file ./app/framework/include/af-types.h
maxValue#
EmberAfDefaultAttributeValue EmberAfAttributeMinMaxValue::maxValue
Maximum allowed value.
Definition at line
121
of file ./app/framework/include/af-types.h