a struct containing the superset of values passed to both emberIncomingMessageHandler on the SOC and ezspIncomingMessageHandler on the host.
Public Attribute Documentation#
type#
EmberIncomingMessageType EmberAfIncomingMessage::type
The type of the incoming message
Definition at line
283
of file ./app/framework/include/af-types.h
apsFrame#
EmberApsFrame* EmberAfIncomingMessage::apsFrame
APS frame for the incoming message
Definition at line
287
of file ./app/framework/include/af-types.h
message#
uint8_t* EmberAfIncomingMessage::message
The message copied into a flat buffer
Definition at line
291
of file ./app/framework/include/af-types.h
msgLen#
uint16_t EmberAfIncomingMessage::msgLen
Length of the incoming message
Definition at line
295
of file ./app/framework/include/af-types.h
source#
uint16_t EmberAfIncomingMessage::source
Two byte node id of the sending node.
Definition at line
299
of file ./app/framework/include/af-types.h
lastHopLqi#
uint8_t EmberAfIncomingMessage::lastHopLqi
Link quality from the node that last relayed the message.
Definition at line
304
of file ./app/framework/include/af-types.h
lastHopRssi#
int8_t EmberAfIncomingMessage::lastHopRssi
The energy level (in units of dBm) observed during the reception.
Definition at line
308
of file ./app/framework/include/af-types.h
bindingTableIndex#
uint8_t EmberAfIncomingMessage::bindingTableIndex
The index of a binding that matches the message or 0xFF if there is no matching binding.
Definition at line
313
of file ./app/framework/include/af-types.h
addressTableIndex#
uint8_t EmberAfIncomingMessage::addressTableIndex
The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.
Definition at line
319
of file ./app/framework/include/af-types.h
networkIndex#
uint8_t EmberAfIncomingMessage::networkIndex
The index of the network on which this message was received.
Definition at line
323
of file ./app/framework/include/af-types.h