Struct that maps actual endpoint type, onto a specific endpoint.
Public Attribute Documentation#
endpoint#
uint8_t EmberAfDefinedEndpoint::endpoint
Actual zigbee endpoint number.
Definition at line
518
of file ./app/framework/include/af-types.h
profileId#
EmberAfProfileId EmberAfDefinedEndpoint::profileId
Profile ID of the device on this endpoint.
Definition at line
522
of file ./app/framework/include/af-types.h
deviceId#
uint16_t EmberAfDefinedEndpoint::deviceId
Device ID of the device on this endpoint.
Definition at line
526
of file ./app/framework/include/af-types.h
deviceVersion#
uint8_t EmberAfDefinedEndpoint::deviceVersion
Version of the device.
Definition at line
530
of file ./app/framework/include/af-types.h
endpointType#
EmberAfEndpointType* EmberAfDefinedEndpoint::endpointType
Endpoint type for this endpoint.
Definition at line
534
of file ./app/framework/include/af-types.h
networkIndex#
uint8_t EmberAfDefinedEndpoint::networkIndex
Network index for this endpoint.
Definition at line
538
of file ./app/framework/include/af-types.h
bitmask#
EmberAfEndpointBitmask EmberAfDefinedEndpoint::bitmask
Meta-data about the endpoint
Definition at line
542
of file ./app/framework/include/af-types.h