CentralScene#

Modules#

central_scene_configuration_t

s_CC_centralScene_data_t_

_cc_central_scene_t

Typedefs#

typedef struct _cc_central_scene_t

Structure that describes a single scene.

Functions#

cc_central_scene_notification_tx(AGI_PROFILE *pProfile, uint8_t keyAttribute, uint8_t sceneNumber, ZAF_TX_Callback_t pCbFunc)

Initiates the transmission of a "Central Scene Notification" command.

void
cc_central_scene_handle_notification_timer(bool start_timer, uint8_t scene_number)

Start or stop Central Scene Notification timer Used when event CENTRAL_SCENE_NOTIFICATION_KEY_ATTRIBUTES_KEY_HELD_DOWN happens.

Returns the array of central scenes.

uint8_t

Returns number of supported scenes.

uint8_t

Returns supported attributes for a given scene.

uint8_t

Gets 'identical' attribute that describes supported key attributes.

bool
cc_central_scene_read(central_scene_configuration_t *pConfig)
bool
cc_central_scene_write(const central_scene_configuration_t *pConfig)

Macros#

#define
CC_CENTRAL_SCENE_SIZE_OF_SUPPORTED_SCENES_ATTRIBUTES sizeof(((cc_central_scene_t *)0)->scene_attributes)

Size of supported scenes.

Typedef Documentation#

s_CC_centralScene_data_t#

typedef struct s_CC_centralScene_data_t_ s_CC_centralScene_data_t

Definition at line 33 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_t#

typedef struct _cc_central_scene_t cc_central_scene_t

Structure that describes a single scene.


Definition at line 42 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

Function Documentation#

cc_central_scene_notification_tx#

JOB_STATUS cc_central_scene_notification_tx (AGI_PROFILE * pProfile, uint8_t keyAttribute, uint8_t sceneNumber, ZAF_TX_Callback_t pCbFunc)

Initiates the transmission of a "Central Scene Notification" command.

Parameters
[in]pProfile

pointer to AGI profile or NULL for lifeline

[in]keyAttribute

The key event.

[in]sceneNumber

The scene number.

[in]pCbFunc

Callback function to be called when transmission is done/failed.

Note

  • Source Endpoint is always set to Root in this function

Returns

  • Status of the job.


Definition at line 55 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_handle_notification_timer#

void cc_central_scene_handle_notification_timer (bool start_timer, uint8_t scene_number)

Start or stop Central Scene Notification timer Used when event CENTRAL_SCENE_NOTIFICATION_KEY_ATTRIBUTES_KEY_HELD_DOWN happens.

Parameters
N/Astart_timer

True if timer should be started, false will stop active timer.

N/Ascene_number

Number of active scene.

App will send notifications periodically as long as the event is active. Frequency depends on whether slow refresh is enabled or not.


Definition at line 73 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_config_get_scenes_attributes#

cc_central_scene_t * cc_central_scene_config_get_scenes_attributes (void )

Returns the array of central scenes.

Parameters
N/A

Note

  • If scenes are identical, the array will contain only one element

Returns

  • Address of the first element in the central scene array.


Definition at line 91 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_config_get_number_of_scenes#

uint8_t cc_central_scene_config_get_number_of_scenes (void )

Returns number of supported scenes.

Parameters
N/A

Returns

  • Total amount of scenes supported by the app.


Definition at line 97 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_config_get_attribute_bitmask#

uint8_t cc_central_scene_config_get_attribute_bitmask (uint8_t scene_number)

Returns supported attributes for a given scene.

Parameters
N/Ascene_number

Number of scene to get supported attributes for

Note

  • This function is used to prepare CENTRAL_SCENE_SUPPORTED_REPORT It is assumption that argument scene_number is higher than 1 only in case when scenes are not identical.

Returns

  • Supported attributes as bitmask


Definition at line 109 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_config_get_identical#

uint8_t cc_central_scene_config_get_identical (void )

Gets 'identical' attribute that describes supported key attributes.

Parameters
N/A

Returns

  • True if all keys are identical, False if different key attributes supported


Definition at line 117 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h

cc_central_scene_read#

bool cc_central_scene_read (central_scene_configuration_t * pConfig)
Parameters
N/ApConfig

Definition at line 18 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/src/cc_central_scene_io.h

cc_central_scene_write#

bool cc_central_scene_write (const central_scene_configuration_t * pConfig)
Parameters
N/ApConfig

Definition at line 20 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/src/cc_central_scene_io.h

cc_central_scene_migrate#

void cc_central_scene_migrate (void )
Parameters
N/A

Definition at line 22 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/src/cc_central_scene_io.h

Macro Definition Documentation#

CC_CENTRAL_SCENE_SIZE_OF_SUPPORTED_SCENES_ATTRIBUTES#

#define CC_CENTRAL_SCENE_SIZE_OF_SUPPORTED_SCENES_ATTRIBUTES
Value:
sizeof(((cc_central_scene_t *)0)->scene_attributes)

Size of supported scenes.

This field advertises the size of each "Supported Key Attributes" field measured in bytes. Note

  • : This value can have values 1-3, but all attributes available in current version of Central Scene (V3) can fit into a single byte.


Definition at line 83 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/CentralScene/inc/CC_CentralScene.h