UserCode#
Modules#
Enumerations#
Typedefs#
Struct used to pass operational data to TSE module.
Functions#
The User Code Set Command used to set a User Code in the device.
The User Code Get ID.
The User Code Report Command can be used by e.g.
The Users Number Report Command used to report the maximum number of USER CODES the given node supports.
Resets the data used by the command class.
Send a Command Class User code support report.
Macros#
Minimum length of a user code as defined in SDS12652.
Maximum length of a user code as defined in SDS12652.
Enumeration Documentation#
user_id_status_t#
user_id_status_t
User ID Status.#
The User ID Status field indicates the state of the User Identifier. All other values not mentioned in below list are reserved for future implementation.
Hex | Description |
---|---|
00 | Available (not set) |
01 | Occupied |
02 | Reserved by administrator |
FE | Status not available |
Enumerator | |
---|---|
USER_ID_AVAILABLE | Available (not set) |
USER_ID_OCCUPIED | Occupied. |
USER_ID_RESERVED | Reserved by administrator. |
USER_ID_NO_STATUS | Status not available. |
57
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
Typedef Documentation#
USER_ID_STATUS#
typedef user_id_status_t USER_ID_STATUS
66
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
SUserCode#
typedef struct SUserCode SUserCode
84
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
s_CC_userCode_data_t#
typedef struct s_CC_userCode_data_t_ s_CC_userCode_data_t
Struct used to pass operational data to TSE module.
93
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
Function Documentation#
CC_UserCode_Set_handler#
e_cmd_handler_return_code_t CC_UserCode_Set_handler (uint8_t identifier, USER_ID_STATUS id, uint8_t * pUserCode, uint8_t len, uint8_t endpoint)
The User Code Set Command used to set a User Code in the device.
[in] | identifier | User Identifier. |
[in] | id | user Id status. |
[in] | pUserCode | pointer to UserCode data. |
[in] | len | UserCode data. |
[in] | endpoint | is the destination endpoint |
Returns
command handler return code
135
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_getId_handler#
bool CC_UserCode_getId_handler (uint8_t identifier, USER_ID_STATUS * pId, uint8_t endpoint)
The User Code Get ID.
[in] | identifier | User Identifier. |
[out] | pId | pointer to return Id. |
[in] | endpoint | is the destination endpoint |
Returns
status valid boolean.
149
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_Report_handler#
bool CC_UserCode_Report_handler (uint8_t identifier, uint8_t * pUserCode, size_t * pLen, uint8_t endpoint)
The User Code Report Command can be used by e.g.
[in] | identifier | User Identifier. |
[out] | pUserCode | pointer to UserCode data. |
[out] | pLen | length UserCode data. |
[in] | endpoint | is the destination endpoint |
a door lock device to send a report either unsolicited or requested by the User Code Get Command. Returns
status valid boolean.
164
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_UsersNumberReport_handler#
uint8_t CC_UserCode_UsersNumberReport_handler (uint8_t endpoint)
The Users Number Report Command used to report the maximum number of USER CODES the given node supports.
[in] | endpoint | is the destination endpoint |
The Users Number Report Command can be send requested by the Users Number Get Command. Returns
maximum number of USER CODES.
178
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_reset_data#
void CC_UserCode_reset_data (void )
Resets the data used by the command class.
N/A |
184
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_SupportReport#
JOB_STATUS CC_UserCode_SupportReport (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, uint8_t userIdentifier, uint8_t userIdStatus, uint8_t * pUserCode, uint8_t userCodeLen, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCallback)
Send a Command Class User code support report.
[in] | pProfile | pointer to AGI profile |
[in] | sourceEndpoint | source endpoint |
[in] | userIdentifier | user identifier |
[in] | userIdStatus | user Id status |
[in] | pUserCode | user code |
[in] | userCodeLen | length of user code |
[out] | pCallback | callback function returning status destination node receive job. |
Returns
status on the job.
198
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
CC_UserCode_Migrate#
void CC_UserCode_Migrate ()
20
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/src/cc_user_code_io.h
Macro Definition Documentation#
USERCODE_MIN_LEN#
#define USERCODE_MIN_LENValue:
4
Minimum length of a user code as defined in SDS12652.
71
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h
USERCODE_MAX_LEN#
#define USERCODE_MAX_LENValue:
10
Maximum length of a user code as defined in SDS12652.
76
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/UserCode/inc/CC_UserCode.h