Transmit complete codes#

Macros#

#define

Transmit OK.

#define

Retransmission error.

#define

Transmit error.

#define

Transmit error.

#define

Security S2. Receiving node has decrypted the frame.

Macro Definition Documentation#

TRANSMIT_COMPLETE_OK#

#define TRANSMIT_COMPLETE_OK
Value:
0x00

Transmit OK.


Definition at line 103 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

TRANSMIT_COMPLETE_NO_ACK#

#define TRANSMIT_COMPLETE_NO_ACK
Value:
0x01

Retransmission error.


Definition at line 104 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

TRANSMIT_COMPLETE_FAIL#

#define TRANSMIT_COMPLETE_FAIL
Value:
0x02

Transmit error.


Definition at line 105 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

TRANSMIT_ROUTING_NOT_IDLE#

#define TRANSMIT_ROUTING_NOT_IDLE
Value:
0x03

Transmit error.


Definition at line 106 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

TRANSMIT_COMPLETE_VERIFIED#

#define TRANSMIT_COMPLETE_VERIFIED
Value:
0x05

Security S2. Receiving node has decrypted the frame.


Definition at line 112 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h