Transmit options for ZW_SendDataMultiEx.

Public Attributes#

uint8_t

< Destination group ID

Transmit options.

Security key to use for sending - only S2 keys are valid.

Public Attribute Documentation#

groupID#

uint8_t _TRANSMIT_MULTI_OPTIONS_TYPE::groupID

< Destination group ID

Reserved


Definition at line 234 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bSrcNode#

node_id_t _TRANSMIT_MULTI_OPTIONS_TYPE::bSrcNode

Transmit options.


Definition at line 236 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

txOptions#

TxOptions_t _TRANSMIT_MULTI_OPTIONS_TYPE::txOptions

Security key to use for sending - only S2 keys are valid.


Definition at line 238 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

securityKey#

enum SECURITY_KEY _TRANSMIT_MULTI_OPTIONS_TYPE::securityKey

Definition at line 240 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h