Radio Profile containing region, baud rate, and wakeup interval for this device.
Public Attributes#
Region in which this system operates.
Wakeup interval for the radio.
Primary Long Range Channel.
Longe Range channel selection mode.
LBT Threshold for Transmit backoff in dBm.
Z-Wave Transmit Power in deci dBm.
Adjustment for antenna gain in deci dBm.
Max transmit power for Z-Wave LR in deci dBm.
Pointer to current HomeID(uint8_t homeID[4]).
Pointer to function called by RF on Rx Completion.
Pointer to function called by RF on Tx Completion.
Pointer to function called by RF on Region change.
Pointer to function called by RF on fatal Assert.
Pointer to structure where to RF Statistics are placed.
Enable radio debugging which is vendor specific.
Pointer to receive handler.
Public Attribute Documentation#
region#
zpal_radio_region_t zpal_radio_profile_t::region
Region in which this system operates.
490
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
wakeup#
zpal_radio_wakeup_t zpal_radio_profile_t::wakeup
Wakeup interval for the radio.
491
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
primary_lr_channel#
uint8_t zpal_radio_profile_t::primary_lr_channel
Primary Long Range Channel.
492
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
lr_channel_auto_mode#
bool zpal_radio_profile_t::lr_channel_auto_mode
Longe Range channel selection mode.
493
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
listen_before_talk_threshold#
int8_t zpal_radio_profile_t::listen_before_talk_threshold
LBT Threshold for Transmit backoff in dBm.
494
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
tx_power_max#
zpal_tx_power_t zpal_radio_profile_t::tx_power_max
Z-Wave Transmit Power in deci dBm.
495
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
tx_power_adjust#
zpal_tx_power_t zpal_radio_profile_t::tx_power_adjust
Adjustment for antenna gain in deci dBm.
496
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
tx_power_max_lr#
zpal_tx_power_t zpal_radio_profile_t::tx_power_max_lr
Max transmit power for Z-Wave LR in deci dBm.
497
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
home_id#
uint8_t* zpal_radio_profile_t::home_id
Pointer to current HomeID(uint8_t homeID[4]).
498
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
rx_cb#
zpal_radio_callback_t zpal_radio_profile_t::rx_cb
Pointer to function called by RF on Rx Completion.
499
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
tx_cb#
zpal_radio_callback_t zpal_radio_profile_t::tx_cb
Pointer to function called by RF on Tx Completion.
500
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
region_change_cb#
zpal_radio_callback_t zpal_radio_profile_t::region_change_cb
Pointer to function called by RF on Region change.
501
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
assert_cb#
zpal_radio_callback_t zpal_radio_profile_t::assert_cb
Pointer to function called by RF on fatal Assert.
502
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
network_stats#
zpal_radio_network_stats_t* zpal_radio_profile_t::network_stats
Pointer to structure where to RF Statistics are placed.
503
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
radio_debug_enable#
uint8_t zpal_radio_profile_t::radio_debug_enable
Enable radio debugging which is vendor specific.
504
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h
receive_handler_cb#
zpal_radio_receive_handler_t zpal_radio_profile_t::receive_handler_cb
Pointer to receive handler.
505
of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h