rf channel statistics structure

Public Attributes#

uint32_t

Transmitted frames on rf channel.

uint32_t

Frame transmit retries on rf channel.

uint32_t

Frame transmit failed by lbt on rf channel.

uint32_t

Frames received with foreign homeid on rf channel.

uint32_t

Frames received with CRC error on rf channel.

int8_t

Background RSSI average on rf channel.

int8_t

End Device RSSI average on rf channel.

Public Attribute Documentation#

rf_channel_tx_frames#

uint32_t zpal_radio_rf_channel_statistic_t::rf_channel_tx_frames

Transmitted frames on rf channel.


Definition at line 476 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_tx_retries#

uint32_t zpal_radio_rf_channel_statistic_t::rf_channel_tx_retries

Frame transmit retries on rf channel.


Definition at line 477 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_tx_lbt_failures#

uint32_t zpal_radio_rf_channel_statistic_t::rf_channel_tx_lbt_failures

Frame transmit failed by lbt on rf channel.


Definition at line 478 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_rx_foreign_homeid#

uint32_t zpal_radio_rf_channel_statistic_t::rf_channel_rx_foreign_homeid

Frames received with foreign homeid on rf channel.


Definition at line 479 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_rx_crc_error#

uint32_t zpal_radio_rf_channel_statistic_t::rf_channel_rx_crc_error

Frames received with CRC error on rf channel.


Definition at line 480 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_background_rssi_average#

int8_t zpal_radio_rf_channel_statistic_t::rf_channel_background_rssi_average

Background RSSI average on rf channel.


Definition at line 481 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rf_channel_end_device_rssi_average#

int8_t zpal_radio_rf_channel_statistic_t::rf_channel_end_device_rssi_average

End Device RSSI average on rf channel.


Definition at line 482 of file /mnt/raid/workspaces/ws.H9QSi59DS/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h