Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

sof#

uint8_t tx_cmd_frame_t::sof

Definition at line 71 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

cmd#

uint8_t tx_cmd_frame_t::cmd

Definition at line 72 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

len#

uint8_t tx_cmd_frame_t::len

Definition at line 73 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

payload#

uint8_t tx_cmd_frame_t::payload[UINT8_MAX]

Definition at line 74 of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h