Public Attribute Documentation#
sof#
uint8_t tx_data_frame_t::sof
Definition at line
79
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
type#
uint8_t tx_data_frame_t::type
Definition at line
80
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp1#
uint8_t tx_data_frame_t::timestamp1
Definition at line
81
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
timestamp2#
uint8_t tx_data_frame_t::timestamp2
Definition at line
82
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
ch_speed#
uint8_t tx_data_frame_t::ch_speed
Definition at line
83
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
freq_no#
uint8_t tx_data_frame_t::freq_no
Definition at line
84
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
rssi#
int8_t tx_data_frame_t::rssi
Definition at line
85
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
sodm#
uint8_t tx_data_frame_t::sodm
Definition at line
86
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
sod#
uint8_t tx_data_frame_t::sod
Definition at line
87
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
len#
uint8_t tx_data_frame_t::len
Definition at line
88
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h
payload#
uint8_t tx_data_frame_t::payload[UINT8_MAX]
Definition at line
89
of file /mnt/raid/workspaces/ws.1eyhFLSdc/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h