Command Class Firmware Update - Bootloader update#
Command Class Firmware Update - Bootloader update.
Macros#
#define
The bootloader target id <1..255:1>
#define
Indicates if the bootloader can be updated.
Macro Definition Documentation#
ZAF_CONFIG_BOOTLOADER_TARGET_ID#
#define ZAF_CONFIG_BOOTLOADER_TARGET_IDValue:
1
The bootloader target id <1..255:1>
If the bootloader update is enabled This determines which target id should be used by the bootloader firmware
Definition at line
31
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h
ZAF_CONFIG_BOOTLOADER_UPGRADABLE#
#define ZAF_CONFIG_BOOTLOADER_UPGRADABLEValue:
0
Indicates if the bootloader can be updated.
Includes the bootloader as a target
Definition at line
40
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h