Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

sof#

uint8_t comm_interface_frame_ptr::sof

Definition at line 53 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/comm_interface.h

len#

uint8_t comm_interface_frame_ptr::len

Definition at line 54 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/comm_interface.h

type#

uint8_t comm_interface_frame_ptr::type

Definition at line 55 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/comm_interface.h

cmd#

uint8_t comm_interface_frame_ptr::cmd

Definition at line 56 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/comm_interface.h

payload#

uint8_t comm_interface_frame_ptr::payload

Definition at line 57 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_serial_api/comm_interface.h