Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
int8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

sof#

uint8_t tx_data_frame_t::sof

Definition at line 79 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

type#

uint8_t tx_data_frame_t::type

Definition at line 80 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp1#

uint8_t tx_data_frame_t::timestamp1

Definition at line 81 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp2#

uint8_t tx_data_frame_t::timestamp2

Definition at line 82 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

ch_speed#

uint8_t tx_data_frame_t::ch_speed

Definition at line 83 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

freq_no#

uint8_t tx_data_frame_t::freq_no

Definition at line 84 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

rssi#

int8_t tx_data_frame_t::rssi

Definition at line 85 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

sodm#

uint8_t tx_data_frame_t::sodm

Definition at line 86 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

sod#

uint8_t tx_data_frame_t::sod

Definition at line 87 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

len#

uint8_t tx_data_frame_t::len

Definition at line 88 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

payload#

uint8_t tx_data_frame_t::payload[UINT8_MAX]

Definition at line 89 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h